To determine the hardware revision and firmware version of an installed safety card:
- Open the setup software Drivegui.
- Type VER * in the terminal screen.
| DIS1-HW | shows the hardware revision |
|---|---|
| DIS1-SW | shows the firmware version |
Réseau d'assistance Kollmorgen
The below represents frequent questions our support, engineering and sales teams have been asked over the years. If you have a question, please submit our contact us form to reach our application engineering team.
To determine the hardware revision and firmware version of an installed safety card:
| DIS1-HW | shows the hardware revision |
|---|---|
| DIS1-SW | shows the firmware version |
The tool "Braking Ramps SafetyGUI" (see Downloads) explains that procedure with an example.
| S300, S400, S600 | With these servo amplifiers, safe reduced speed can be realized with external components. Different proposals for cat. 2 and cat.3 are given on page Safe Reduced Speed. |
|---|---|
| S700 | With the built-in Safety expansion card the function SLS (safely limited speed) is integrated in the servo amplifier, see page Safety Concept S700. |
It is possible to connect several servo amplifier STO inputs to one output of a safety control and SIL2/PLd can be met.
A maximum of 9 amplifiers can be connected to one output.
For more information see page S700 Safety: Several S700 on one safety control
This occurs because the setup software is resetting "Motor with Brake" to "Motor without Brake".
Fix: Use the terminal screen and enter the ASCII commands MBRAKE1 HSAVE.
Explanation: The motor options are saved in the ENDAT encoder. If this information is wrong, the brake option in the drive is always reset.
| Motor Size | Type | Resolution |
|---|---|---|
| AKM 2/3/4 | AD36 | 19 Bit |
| AKM 5/6/7 | AD58 | 22 Bit |
The 5V type is always used.
AA always describes a single turn type and AB a multi turn type.
| S600 | "PROFIBUS" printed on the front cover |
| S300/S700/S600 | "PROFIBUS DP" printed on the front cover |
The only required setting is the address.
The Profibus chip will detect the baud rate automatically. It can not be set on the drive.
Special for the S400: If the field bus address (ADDRFB) has been set to zero, the drive will be addressed via the general address that has been assigned by the S400 master.
To start several drives synchronously, it can be useful to prepare the motion tasks via the bus but start them via a digital input. Refer to page Start of Motion Tasks in PROFIBUS operation.
See page Speed set point via fieldbus system.
S300: 2.1
S400: 2.1
S600: 2.1
S700: 2.1 and 2.2
All amplifiers can work with 2.2 protocol in compatibility mode 2.1.
The SinCos amplitude monitoring enables the F04 error with:
Solution: connect the encoder, check the cable
This error occurs with new encoders, that have never been initialized
Solution: Initialize the data with the command HSAVE (terminal screen)
Feedback cable shielding
Solution: see Sporadic Error Message F04 with Linear Measuring Systems
See pages Supervision of Sine Cosine Encoders, Setup of an Endat or Hiperface or BISS encoder, and AKD LED Display or Servostar LED Display.
See page SSI Encoder Evaluation.
See page Positioning with external SSI encoder.
To change direction you must exchange sine and cosine.
For more information refer to Motion direction - Parameters.
Direction of Hall signals are inverted with the command HALLDIR 1 (S300). Please observe, that this inverts the primary feedback, too. Change DIR from 21 / 20 to DIR 84 / 85 in this case.
For more information refer to Motion direction - Parameters.
The following BiSS-C encoders are known to work with an AKD drive. This list does not include BiSS Mode B encoders, which function differently.
| Encoder | Name | BISSBITS | Sine Cycles per Rev or Pole Pitch (FB1.ENCRES) |
| LMA10-xx-xxB-xx-x-03 | LMA10 Magnetic Encoder, option 03, from RLS | 26 | (pole pitch / encoder bit resolution) * 64 |
| S-9SRH-0398 | Renishaw Rotary Encoder | 32 | 4294967295 |
| RL 26B / RL 32B / RL 36B | Renishaw RESOLUTE Linear Encoder | 26/32/36 | (pole pitch / encoder resolution) * 2^(32-BISSBITS) |
| RA 18B / RA 26B / RA 32B | Renishaw RESOLUTE Rotary Encoder | 18/26/32 | 4294967295 |
| AD36-0019 / AD58-0022 | HENGSTLER Rotary Encoder (Single-turn) | 19/22 | 4294967295 |
| AD36-1219 / AD58-1222 | HENGSTLER Rotary Encoder (Multi-turn) | 31/34 | 1048576 |
Configuration requires that FB1.SELECT be manually set to 34, and that FB1.BISSBITS and FB1.ENCRES be set according to the values/equations in the table above.
Full Setup Procedure for a BiSS-C Encoder:
See page Setup AquadB 5V encoder