Speed set point via fieldbus system
Valid for S300, S400, S600, S700
Task:
A speed set point shall be delivered digitally via a bus system. It must be possible to adjust the speed setpoint by an offset voltage with an analog input..
Setup
VSCALE1
Object 297, scaling turns / 10V for analog input
Settings in the setup software
OPMODE
1: Velocity analog
I/O analog set point function
4: Xsoll = SW1 + SW2
Example
A speed offset of +/- 10rpm shall be realized with analog input 2.
Scaling for analog input 2 must be set to 10rpm/10V and a scalable voltage supply of +/-10 V is wired to input 2. All further settings must be done according to the list above.
Analog input 1 must be supplied with a constant voltage in the range between 0 to 10V. Set VSCALE1 to 2 and supply 0V to input 2. Now the auto-offset function for analog input 1 can be started. The speed setpoint is given by parameter VSCAL1, scaling according to the constant voltage applied.
Home >
Knowledge Base >
FAQs >
Downloads >