Motion direction - Parameters
Valid for S300, S700
Table of Contents
There are several parameters to change the motion direction.
Parameter DIR
The DIR variable defines the count direction for feedback information. The DIR variable is a 16bit variable, the single bits define the count direction for different feedback units.
| DIR (dec, default) | 21 | ||||||||||
| Bit 10 | Bit 9 | Bit 8 | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |
| DIR (bin, default) | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 | 0 | 1 |
| Feedback | Analog Hall | Absolut Information |
Commutation | Electr.Gearing | Second Feedback |
Primary Feedback |
|||||
| Wert 0 | Standard | Standard | Standard | Standard | ccw | ccw | |||||
| Wert 1 | ccw | ccw | ccw | ccw | cw | cw | |||||
Parameter HALLDIR
For the use of HALL Sensors there are 2 tables with hall segment numbers.
| HALLDIR (default) | 0 | see ((Hall Sensors)) |
| Feedback | Digital Hall | |
| Wert 0 | Standard | order of hall segments 1,5,4,6,2,3 |
| Wert 1 | ccw | order of hall segments 1,3,2,6,4,5 |
Notice: If HALDIR has been changed from 0 to 1, bits 0 and 6 of Parameter DIR need to be changed. DIR 21 must become DIR 84, DIR 20 must become DIR 85.
Parameter ENCOUT
ENCOUT defines the number of lines that are given out by the EEO (incremental encoder) interface for one turn of a rotary motor or one pole pitch for a linear motor. Negative values are used to invert the output direction.
| ENCOUT (default) | (+)1024 |
| Function | Encoder Emulation |
| sign + | Standard |
| sign - | ccw |
Parameter VSCALE1
If the analog input 1 is used as the setpoint input for velocity control, then the VSCALE1 parameter is used to scale the input voltage.
| VSCALE1 (default) | (+)3000 |
| Function | Analog Set Point |
| Sign + | Standard |
| Sign - | ccw |
Home >
Knowledge Base >
FAQs >
Downloads >