Skip to main content
Success Story | 2 minute read

V-TAB uses AGVs to minimize damage to paper rolls.

V-TAB, Sweden’s largest printing conglomerate, has built a new newspaper printing plant outside Gothenburg where they currently print four different newspapers. Automated Guided Vehicles (AGVs) based on technology from Kollmorgen are used in the printing process to minimize damage to the paper rolls.

The AGV system together with the Warehouse Management System (WMS) was supplied by Rocla, one of Kollmorgen’s channel partners supplying AGV systems based on Kollmorgen’s AGV controls technology. The AGV system was taken into operation 2010 and consists of two AGVs. The system transports paper rolls from the strip station, where the brown wraps are stripped from the paper rolls, to a temporary storage. The temporary storage is filled with paper rolls to be used during the day/night. Rocla’s AGVs also transport paper rolls from the temporary storage to the printing presses when new rolls need to be loaded.

‘The benefit of using AGVs instead of manual forklifts or floor conveyors is that you ensure that there will be no damage to the paper rolls during transportation. AGVs are very accurate and pick up, transport, and unload paper rolls with high precision’, says Hans-Åke Stjernman, System Engineer at V-TAB. ‘This leads to lower operational costs due to less damage to paper rolls and infrastructure and fewer interruptions in the printing process.’ Hans-Åke Sjernman was a member of the evaluation team that considered different transportation methods and suppliers.

Kollmorgen, a leading manufacturer of driverless control technology, and Rocla Oy, a leading AGV system supplier, are strategic global partners in applications for automated transportation based on Kollmorgen’s AGV controls technology. Kollmorgen control solutions are applied in more than 17,000 AGVs around the globe. Kollmorgen’s AGV control solution promises lower total costs for system integrators and end-users. It is applicationsindependent, scalable and works with all AGVs, from the small and simple to the big and complex. It is also easy to integrate with host systems and material handling systems, and because the same platform is used everywhere, the same engineering skill set applies for all types of applications.

View the video:

Loading

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.