Skip to main content
Success Story | 2 minute read

StoVerotec

STOVEROTEC INCREASE EFFICIENCY IN A COLD, HUMID ENVIRONMENT WITH TECHNOLOGY FROM KOLLMORGEN

StoVerotec have minimized their internal transportation costs by automating the transportation of polystyrene blocks from the production area to the warehouse. Automated Guides Vehicles (AGVs) from Barbieri & Tarozzi using vehicle automation technology from Kollmorgen, handle loads up to 6 meters high in a non-acclimatized warehouse exposed to the continental climate of South Germany.

The German company Sto AG is one of the world leaders in thermal insulation of facades and interiors in both existing and new buildings. Their subsidiary StoVerotec GmbH has a factory in Lauingen where polystyrene panels are produced. The Italian company Nuova Idropress S.p.A. supplied all the production plant for the polystyrene blocks, including the Automated Guided Vehicles (AGVs) used to transport the blocks from the production line to the warehouse and the cutting line. Using AGVs provides a safer and more efficient operation, giving optimized output yields.

SITI – Barbieri & Tarozzi Group has implemented an AGV system which is capable of coping with StoVerotec’s demanding environment. The system is based on the AGV control solution from Kollmorgen that supports multiple navigation technologies and severe environments. The laser navigation sensor (LS5) is designed for rough conditions in the cold and wet, down to -30°C and up to +50°C, with no optical condensation at 95% relative humidity, leading to endless business opportunities. StoVerotec’s demanding environment was a clear case for an AGV system. SITI – Barbieri & Tarozzi Group successfully designed an AGV system that can:

  • transport loads as high as 6.2 meters
  • store high-density polystyrene blocks in the warehouse into deep stacking in narrow aisles
  • cope with the tough environmental conditions with high humidity and low temperatures

Thanks to the technology from Kollmorgen an AGV system with dual navigation technologies could be designed. In open areas the AGV uses laser navigation while in the narrow aisles it switches over to magnetic navigation. ‘Kollmorgen’s components designed for rough environments and the concept of multi-navigation made it possible for us to design an AGV system for this demanding environment’, says Fabrizio Bertacchi, Sales Area Manager at SITI – Barbieri & Tarozzi Group. He goes on: ‘The cooperation with Nuova Idropress and Kollmorgen, both top-level suppliers, gives us a elevant reference in such markets as the polystyrene one’.

The system currently consists of three vehicles operating 16 hours/day although the system is designed to operate 24/7. ‘Both design and commissioning went smoothly thanks to efficient design and the service tools. The alternative to AGVs would have been two manual forklifts operating in two shifts’, says Andrea Marazzoli, the electrical engineer responsible for AGV technology at SITI – Barbieri & Tarozzi Group. ‘This state of the art technology has been applied with full success and the plant reached full efficiency in the production of EPS panels at StoVerotec in Lauingen’ says Mr. Frithjof Koerdt, StoVerotec’s Production and Technical Director. Kollmorgen’s control solutions are applied in more than 17,000 AGVs around the globe.

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.