Skip to main content
Success Story | 2 minute read

Reliable and Consistent Supply of Motion Systems

Kollmorgen Helps Rapidly Scale CT Scanner Production

Challenge

When the world became aware of the COVID-19 outbreak first identified in Wuhan, China, it quickly became clear that greatly increased diagnostic capacity would be needed to understand the effects of the disease and guide treatment for an anticipated surge in patients. Over the next several weeks, that surge would spread around the world, and doctors would come to understand that the disease’s effects could be more widespread and unpredictable than initially thought.

A computerized tomography or CT scan combines a series of X-ray images taken from different angles around the body, digitally processed to create a 3D representation of organs and tissues throughout the body. CT scanners are an important tool in understanding how COVID-19 affects the lungs, circulatory system, kidneys, nervous system and more.

Early in the outbreak, one of the world’s largest producers of diagnostic equipment—and a leading supplier of CT scanning equipment in China—reached out to Kollmorgen for help ramping up production to address the rapidly growing crisis. It soon became clear that the pandemic would spread worldwide, and hospitals in every region would need to augment their diagnostic capabilities—creating even greater pressure to deliver on a rapidly growing volume of CT scanner orders.

Solution

The detail and clarity of CT images depends on the motion systems that control the positioning of the X-ray technology. This major producer of CT scanners has a reputation for achieving image resolution well beyond the competition while minimizing patient exposure to ionizing radiation. It has achieved these market-leading results in part through a long-standing relationship with Kollmorgen, relying on industry-leading servo systems and motion expertise to achieve superior speed, control and precision.

To meet the sudden and extreme increase in demand, a team of Kollmorgen sales and operations leaders from across Asia, Europe and North America convened in early 2020 to define the strategy and tactics for success.

The team quickly identified opportunities in both Asia and North America to adjust priorities and production schedules in order to supply the volume of AKM motors, AKD drives, cables and motion subassemblies required to meet the critical demand.

Results

Kollmorgen has supplied motion solutions to high-end medical device manufacturers for more than two decades. As the pandemic broadened in scope and intensity, many of these companies have relied on Kollmorgen’s expertise, global capabilities and can-do approach to help them mount an effective response. For this particular manufacturer of CT scanners:

  • Kollmorgen answered the call to increase supply of servo motors and other components globally, increasing production by 62% in just eight weeks.
  • With Kollmorgen’s support, the manufacturer was able to respond to the COVID-19 crisis in its very early stages, and in the region that was first affected by it.
  • As the pandemic spread across the globe, Kollmorgen has helped the manufacturer respond effectively in every region.

Kollmorgen has also supported a similar accelerated production schedule for a number of other key medical device manufacturers worldwide who provide CT scanners for both hospitals and mobile care.

“Kollmorgen is a well-known provider of motion solutions for critical medical diagnostic technology, and our precision and reliability have played a significant role in the advancement of CT scanning. We’re extremely proud to support the world’s leaders in CT imaging equipment and to contribute to the fight against COVID-19 with the rapid production scale-up required to meet new levels of global demand” - Mike Crowe, Vice President of Sales, Medical, Kollmorgen

Learn More

Ready to design and build a more ambitious machine?

Learn more Talk to a Motion Expert Explore Our Design Tools

 

About Kollmorgen

Kollmorgen has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, linear actuators, gearheads, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…
Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite

Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite >

Step into the future of surgical robotics and enhance your understanding of what’s possible. This webinar offers a detailed exploration of the cutting-edge components that drive precision and efficiency in today's advanced surgical robots.
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Kollmorgen Motors for Medical Imaging: Proven Processes, Reliable Delivery >

Few business challenges are as formidable as designing, manufacturing and delivering medical imaging equipment to healthcare organizations around the world. From mechanical and electrical components, to communication and control systems, to motion…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production

Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production  >

One important stage in manufacturing lithium-ion batteries for electric vehicles is seal-welding the positive-terminal top cap to the battery shell. Laser welding is the ideal technology for this purpose, but it requires precise motion, speed and…
Kollmorgen Azure Surgical Robotics Story

Enabling New Surgical Possibilities with High-Torque, Low-Temperature and Compact-Size Motors >

A new collaborative surgical robot helps surgeons do their best work, in more types of surgery, delivering better outcomes. TBM2G servo motors make it possible.