Skip to main content
Success Story | 2 minute read

In late 2021, a team with strong academic, industrial and medical credentials joined forces to form Azure Medical Innovation Corporation. Their vision was to develop next-generation collaborative surgical robots to assist physicians with interoperative surgical navigation in a medical metaverse concept.

Challenge

To keep pace with the customer demand and the changing technical requirements for their surgical robotic arms, Azure Medical Innovation Corporation faced both technical and speed-to-market challenges.

First, the company’s surgical robot arms needed to meet their customers’ specific technical specifications for a very compact design, including overall payload capacity, envelope size, Degrees of Freedom, and stable torque output. In addition, the arms had to offer maximum utility and versatility with low noise and operating temperature, and fully integrated control of the robot and instrument cluster.

The Azure team was also faced with the need for quick prototyping and accelerated speed to market. Their engineers had to ensure they could transform their customers’ varying specifications into functional and customized robotic arms, often within six months.

“The high power and performance density were important reasons why we used these motors. Surgical applications usually require robots with smaller form factors to fit into the tight space around the bench together with other instruments. Low noise, reliability and efficiency leading to low operating temperature are also reasons that make TBM2G more suitable for medical applications.
—Dr. Ning Li, Chief Technology Officer

Solution

Working closely with Kollmorgen engineers, Azure specified TBM2G motors for their surgical robotic arm designs. The TBM2G motors allowed the final working arms to be 20% smaller than those in similar-sized motors due to its higher torque density.

Even the smallest of the standard seven TBM2G frame sizes allows for 24.7mm motor thru bore throughout to accommodate cables, pneumatics, and fluid tubing to maximize the utility and versatility of the compact robotic arm. The arm can be easily customized to suit the workspace and configuration requirements of specific surgical applications.

To expedite delivery times, Kollmorgen completed prototypes two months quicker than competitors. Using a standard TBM2G motor with standard strain wave gearing delivered a modular joint design that further reduced production schedules.

Kollmorgen Azure application image

Results

The shorter stack design of TBM2G helps to reduce the robot design size by 30%. Its high torque density ensures low temperature rise with high payload during active motion, making it perfectly suited for surgeries that require multiple instruments. And its electro-magnetics are optimized for strain wave gearing to deliver more ability to create powerful robots that can help surgeons do their best work, in more types of surgery, delivering better outcomes for their patients.

 

Featured Product

TBM2G motors are optimized to meet the typical size, weight, speed, torque and temperature requirements of high-performance, high- precision applications such as collaborative robots in the 15 kg and under class. By meeting key performance goals with the shortest and lightest electromagnetics package, engineers can achieve faster, smoother robotic movements with lower joint weight, higher load capacity, greater energy efficiency and lower thermal rise.

Kollmorgen TBM2G

Download as PDF

Incorporating Frameless Motors Into an Environmentally Resilient Design

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to learn how.

Learn More

Achieving Ultimate Motion Precision Using Frameless Servo Motors

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in your mechanism.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite

Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite >

Step into the future of surgical robotics and enhance your understanding of what’s possible. This webinar offers a detailed exploration of the cutting-edge components that drive precision and efficiency in today's advanced surgical robots.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…
Signs You Should Consider a Frameless Motor in Your Machine

Signs You Should Consider a Frameless Motor in Your Machine >

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions?
English, IN
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…