Skip to main content
Success Story | 2 minute read

Universal Robots - Articulated-Arm Robots - Better motors for more options

The UR5 and UR10 are two models from Universal Robots intended to advance the flexibility of articulated-arm robots in industrial production. The focus is on work areas where conventional robots have proven to be too big, too expensive and too loud. Due to their low weight, the UR5 and UR10 can be used wherever they are needed.

A large part of the power density of these six-axis articulated robots comes from specially adapted KBM motors from Kollmorgen. Universal Robots was able to embed the motors directly into the articulation axes without the need for additional housings.

Universal Robots developed the UR5 and UR10 models for small- and medium-sized enterprises in particular. The handling units lift a payload of 5 and 10 kilograms while themselves weighing only 18 and 25 kilograms respectively. This low weight, without complex subcomponents, makes it possible to move the units easily.

These multi-functional, six-axis robots are also flexible in operation given their user-friendly software. They are ready to perform new tasks in no time, with no special knowledge of robotics required for programming.

Modular Design

The exceptional ratio of dead weight to loading capacity is achieved through a sophisticated, lightweight design that does not contain anything it does not need.

This minimalist strategy means integrating Kollmorgen’s frameless motors directly into the articulation axes. The robot itself takes on the function of the motor housing, while the gear unit simultaneously serves as the primary bearing of the rotor.

Viewed as a whole, the components used by Universal Robots frequently take on multiple functions. This considerably reduces the number of mechanical components such as ball bearings, couplings and shafts, thus decreasing overall system weight and form factor. In addition, with their high power density, Kollmorgen KBM motors increase the lifting capacity of the UR5 and UR10 platforms.

The KBM motor series offers advanced electromagnetic designs for optimized torque and minimal cogging and harmonic distortion. These benefits are offered over a large operating speed range. The electromagnetic technology, with high packing density in the stator, increases torque and keeps thermal losses low.

High-strength rare earth magnets are used in the rotor, enabling a continuous torque range of 1.45 to 3,445 N·m across the KBM series along with a peak torque range of 4.91 to 12,812 N·m. “The high quality of these motors was a reason why we opted for Kollmorgen,” explains Esben H. Østergaard, technical business manager of Universal Robots.

With KBM motors embedded in the robot housing and directly driving the load, the robots are able to achieve a high level of precision in movement and force control. Targeted force control is critical in this regard because the robots constantly have to move highly variable workpieces perfectly.

In practice, the robots recognize the size and elasticity of objects and adjust the force to be applied accordingly. This force must be stronger than just 25 N to accomplish this. With a precision of ± 10 N and an accuracy of ± 5 mm, the required force and desired position can be programmed and executed for each of the six joints.

Esben H. Østergaard, Universal Robotics
Esben H. Østergaard, technical business manager of Universal Robots

Operation without noise but with high energy efficiency

These robots also offer the advantages of low noise and energy-saving operation. From a total-cost-of-ownership perspective, the economical use of resources directly increases the efficiency of the robots and thus the competitiveness of the technology.

As an additional benefit, high energy efficiency is linked to reduced losses in the motors. Less heat is produced, so the motors stay cooler, operate below their maximum ratings, and consequently achieve a longer service life. This improved thermal behavior also prevents the entire construction from heating up.

“The motors we used in the past became pretty hot when in continuous operation. Because of the lower losses, the KBM motors from Kollmorgen simply stay colder,” Østergaard explains, referring to test procedures with long operation periods and comparatively high loads.” We can therefore run our robots in continuous operation without derating.”

In the KBM series, Kollmorgen provides an innovative direct drive frameless motor technology. These frameless motors offer mechanical and plant engineering a wide range of solutions for creating applications with a maximum degree of flexibility, power density, dynamics and durability.

In addition to these technical advantages, the KBM platform includes 14 frame designs and many pre-engineered standard options with competitive lead times. “We can basically order as many motors as we want, when and how we want,” emphasizes Østergaard. This aspect is of particular importance because Universal Robots is growing strongly.

“We therefore need a partner in motion technology who is a good fit for us,” he adds. In this regard, Kollmorgen was able to impress the Danish robot specialists with reliable delivery and has since established a Universal Robots-specific production line at the Czech location in Brünn.

KBM Direct drive inside

Prospects

Ultimately, the quiet operation and high quality control of KBM synchronous servo motors ensure that the robots can be used outside of handling applications, too. Up until now, the focus of Universal Robots has been to use robots as a tool for performing simple tasks.

“We are therefore not competing directly with other robot manufacturers who deal with more complex tasks. Instead we are saving people from having to perform tiring, monotonous manual work,” stresses Østergaard. However, as the company from Odense has developed light constructions without uncontrollable oscillations and vibrations, new application possibilities emerge such as with welding and gluing.

“We can expand our business channels,” says Østergaard. This development is accompanied by the fact that — due to sophisticated safety technology — both robot models are even able to be employed without additional shielding. This opens the path to safe and comfortable cooperation between staff and technology.

Kollmorgen KBM and Universal Robotics

About Kollmorgen

Kollmorgen, a Regal Rexnord Brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Download as PDF

Exoskeleton

From the promise of greater freedom and mobility among aging populations to empowering human performance in industrial applications, the demand for exoskeletons is significantly rising. But effectively emulating human movement, safely, is a challenge.
Learn More

Exoskeletons at Scale: Accelerating the Transition from R&D to Full-rate Production

The exoskeleton market is still in its infancy — but evolving quickly and ripe with opportunity. It’s a double-edged sword for OEMs who must identify the most impactful applications and crack the code on full-scale production, which presents a new set of challenges and considerations.

Projects that seemed feasible during R&D and even LRIP can quickly become impossible at scale for a variety of reasons. So how can OEMs foresee (and avoid) issues that may arise as they ramp up production? Here, we’ll cover key tips and insights.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Explosion-proof technology helps create a safety shield for heavy-duty AGVs 

Explosion-proof technology helps create a safety shield for heavy-duty AGVs >

The AKME servo motor series with ATEX certification enables heavy-duty AGV development for hazardous locations in chemical, painting, polishing and specialized facilities.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Designing Field Robots for Harsh and Unpredictable Environments

Designing Field Robots for Harsh and Unpredictable Environments >

This session explores how innovative technologies from Kollmorgen and Regal Rexnord’s broad portfolio of motion control technologies can help engineers meet the rigorous demands of field robotics.
Motion Control Principles for Scalable Humanoid Robotics

Motion Control Principles for Scalable Humanoid Robotics >

As humanoid robotics gain momentum across industries—from logistics and manufacturing to healthcare and public safety—the demand for precise, efficient, and scalable motion control solutions is accelerating. Engineers face complex challenges in…
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…