Skip to main content
Success Story | 2 minute read

Automating Metal Forming Systems to Improve Productivity and Flexibility

A leading machine builder in Italy supports more than 1,500 factories worldwide, providing manufacturing solutions for chimney pipes, air conditioning, automotive, medical and pharmaceutical applications. With growing demand for new pipe shapes and sizes, the company sought to position its machine as the preferred choice for metal-forming flexibility and productivity.

Challenge

The machine builder engaged Kollmorgen to collaborate on its new design, with a particular focus on the mechanism driving the spindle and positioning axes. The goal was to strongly differentiate the machine through enhanced acceleration, precision, productivity and the flexibility to enable highly customized and automated processes.

The original machine’s performance was limited by conventional rotary motors, gearboxes and belts that needed frequent adjustments to accommodate the various pipe diameters and lengths. Resonant frequencies associated with the mechanism’s belt tension degraded cut quality and required manual intervention, which increased production time and material waste.

The challenge was to eliminate these issues to improve precision and maximize the time the machine was producing parts, while also achieving greater flexibility to address the market demand for expanded pipe-forming capabilities.

“Cut quality has improved without the need for manual intervention to adjust spindle speed due to belt tension problems. Optimal cut speeds can be achieved based on material and part size.”
—Angelo Trombetta Motion Solutions Consultant Kollmorgen Italia

Solution

Kollmorgen engineers suggested a direct drive approach to eliminate productivity and quality limitations due to the use of gears and belts, which cause system compliance issues that prevent quicker moves and reduce cut precision. Further collaborative engineering led to the choice of a KBM Series direct drive motor for incorporation into the machine’s spindle. The frameless motor’s large thru bore diameter provided a unique innovation opportunity by enabling an automatic centering capability to adjust quickly for tubes of different sizes.

Kollmorgen identified the optimal solution to minimize machine cut time. The design of the new machine makes it more flexible and compact, ensuring stable performance that remains constant over time, with no downgrade even through a high number of cycles. The solution enhances performance and adds design flexibility to accommodate the varied pipe diameters and lengths demanded in the customer’s markets.

Automating Metal Forming Systems to Improve Productivity and Flexibility-image2

Results

A collaborative approach between Kollmorgen and the customer transformed the company’s machine capabilities to deliver a higher level of performance, precision and accuracy.

  • Dramatic improvements in precision, rigidity and acceleration have resulted in productivity increase of 20%.
  • Improved cut quality has enabled a reduction in material waste.
  • A more flexible machine design accommodates pipe diameters of 60 – 820 mm and lengths up to 1550 mm without time-consuming manual adjustments.
  • Quick and reliable setup has minimized changeover time for new pipe sizes and allowed for automated setup using an optional robotic loader.

Automating Metal Forming Systems to Improve Productivity and Flexibility-image3

About Kollmorgen

Kollmorgen, a Regal Rexnord Brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Download as PDF

Incorporating Frameless Motors Into an Environmentally Resilient Design

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to learn how.

Learn More

Achieving Ultimate Motion Precision Using Frameless Servo Motors

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in your mechanism.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Robotic Arm Actuators for Articulated Motion

Optimizing Robotic Arm Actuators for Articulated Motion >

Why robotic arm actuator performance depends on more than motor selection, and how to optimize performance at the system level.
Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Minesweeping UGV

Frameless Motors for Military Minesweeping UGVs: Power, Size & Reliability >

Frameless motors for tracked Unmanned Ground Vehicles (UGVs) in minesweeping maximize torque density, reduce size and ensure reliable performance in extreme environments.
How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market

How to Select the Right Motor for Robotic Applications to Reduce Cost and Time to Market >

Understanding the physics and optimization techniques of electric motors— including slotted, slotless, and frameless designs— is essential for enhancing value and performance. In this webinar, we’ll discuss the effects of pole count, winding…
Signs You Should Consider a Frameless Motor in Your Machine

Signs You Should Consider a Frameless Motor in Your Machine >

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions?
English, IN
Incorporating Frameless Motors Into an Environmentally Resilient Design

Incorporating Frameless Motors Into an Environmentally Resilient Design >

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to…
Achieving Ultimate Motion Precision Using Frameless Servo Motors

Achieving Ultimate Motion Precision Using Frameless Servo Motors >

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in…