Skip to main content

Meeting the ‘got milk?’ challenge in Europe's dairies >

Europe's second largest dairy company, Arla Foods, has been using AGVs in their facilities since 2009. Read more to see how Arla Foods ensures everyone "gets milk."

AGVs in the new industrial landscape >

The next generation of industries is facing new challenges. What role can Automated Guided Vehicles play?

Tips on How to Confidently Set Up Your Linear Motor System >

Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications.  In order to achieve the highest level of performance, the linear motor system must be commissioned…

Issues to Consider when Operating a Motor in a Vacuum >

Question: I need to operate a servo motor in a vacuum, what are some considerations?  Answer: In a word?  Outgassing.  You might think that proper motor sizing is a big issue, it always is, however if you can't conform to the other…

Meet a real pioneer in laser-guided AGVs >

In the mid-1970s, Tetra Pak started to use AGVs (automated guided vehicles) in their manufacturing and warehouse facilities.

Key Tips on Dealing with 64-bit data on Modbus Communications Devices that only Support 32-bit data >

Most of the AKD drive’s parameters have a 32bit data size, but some parameters have a 64bit data size.  Modbus communication on the AKD drive uses registers of a 16bit data size.  So for a 64bit parameter, it takes four registers to send…

That's One Small Step... 0.9 vs 1.8 Degree Step Angle >

There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors.  Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…

Going Small - How Current Step Motor Technology Can Help You Reduce Machine Size >

As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…

Getting the Best Performance from Encoders >

I often see some confusion in various customers’ minds regarding encoder performance with automation systems which have servo drives or variable frequency drives (VFD). Some customers feel that when they are providing best in class encoders,…

Applications Sizing - Part 1: Getting Started Sizing Servos >

Never sized a servo before? Well, we want to share with you some of the best practices we have found over the years. Over the next few months, we will continue this series with a variety of tidbits that will help you become more comfortable with the…

Eccentricity, Wobble, and How a Servo System Can Help >

By definition, Eccentricity is a measure of how much a roll deviates from being perfectly circular. Ideally, eccentricity should be zero, but in reality, it is never zero. Practically not a single roll is a perfect circle because it is produced using…

4 Tips for Considering Your Servo Motors IP Rating in Your Application >

What should you consider when factoring IP Rating into your specification and what other environmental factors should be considered when specifying motion products? As a manufacturer of motion control products for a variety of markets, Kollmorgen…