Europe's second largest dairy company, Arla Foods, has been using AGVs in their facilities since 2009. Read more to see how Arla Foods ensures everyone "gets milk."
Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications. In order to achieve the highest level of performance, the linear motor system must be commissioned…
Question: I need to operate a servo motor in a vacuum, what are some considerations?
Answer: In a word? Outgassing. You might think that proper motor sizing is a big issue, it always is, however if you can't conform to the other…
Most of the AKD drive’s parameters have a 32bit data size, but some parameters have a 64bit data size. Modbus communication on the AKD drive uses registers of a 16bit data size. So for a 64bit parameter, it takes four registers to send…
There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors. Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…
As it turns out, "going small" is an effort that traces back to the first steppers ever manufactured. Released in 1952, the Sigma "Cyclonome 9" series, one of the first steppers ever designed, was the first standard offering of its kind. Motors had a…
I often see some confusion in
various customers’ minds regarding encoder performance with automation systems which
have servo drives or variable frequency drives (VFD). Some customers feel that when they are
providing best in class encoders,…
Never sized a servo before? Well, we want to share with you some of the best practices we have found over the years. Over the next few months, we will continue this series with a variety of tidbits that will help you become more comfortable with the…
By definition, Eccentricity is a measure of how much a roll deviates from being perfectly circular. Ideally, eccentricity should be zero, but in reality, it is never zero. Practically not a single roll is a perfect circle because it is produced using…
What should you consider when factoring IP Rating into your specification and what other environmental factors should be considered when specifying motion products?
As a manufacturer of motion control products for a variety of markets, Kollmorgen…