Skip to main content
blog | When will my AGVs turn into money machines? |
|
2 minute read

When will my AGVs turn into money machines?

This is the question every AGV buyer wants an answer to. Automated guided vehicles (AGVs), such as mobile robots and carts, often give a high return on investment (ROI) with a payback period of only 1-2 years. Here is a general description of how to calculate the point in time when you can expect years of profits ahead of you—and where to turn for further advice.   

Many things to consider

The accuracy of your investment calculation will depend on the precision of your input.

To start your investment calculation, you need to consider the following:

  • Daily transport flows including seasonal variations (check your WMS)
  • Bottlenecks such as pick up and drop off stations
  • Load types and load carrier types
  • Site conditions and organizational experience from implementing AGVs

The return on investment also depends on what kind of business you are in. AGVs perform best at even workflows where waste as a result of empty driving is reduced to a minimum. You can use AGVs in a wide variety of industries and get quick and significant efficiency gains. In the e-commerce sector, you also need to consider what the potential for fast expansion with AGVs (versus fixed automation) is worth to your company.

Getting a rough indication

You can calculate the return on investment and payback period for AGVs in many ways. Our channel partners Rocla and Transbotics have put together value calculation tools for AGVs. Test the Rocla calculator and the Transbotics calculator for a first ROI indication. We are also a member company of MHI, who has put together an excellent presentation for businesses thinking about buying AGVs.

The way to the best answer

Every manufacturing plant or warehouse is unique. Our channel partners can give you the detailed ROI calculation you need for an investment decision and take the project to the next level with simulations, test installations and reference site visits. Talk to them directly or go via us to find the right partner to work with depending on where you are and what you do. Don’t forget to subscribe to our newsletter to strengthen your knowledge of AGVs.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…