Skip to main content
blog | Speeding up installation by redefining the rules |
|
2 minute read

Speeding up installation by redefining the rules

The lack of service engineers makes quicker design and commissioning of automated guided vehicles (AGVs) a hot topic in the automation industry. A new type of software with the potential to remove time-consuming tasks, such as defining traffic rules for AGVs is now on the market.  

New level of control

Designing traffic rules for AGVs is a challenge – whether you are dealing with small carts, mid-sized mobile robots or large 16-wheelers. You need to avoid traffic jams in each AGV cluster, but still open up for flexible and efficient vehicle movements from different places in your manufacturing plant or warehouse. What is more, the challenge grows as the number of AGVs in your system increases.

NDC Solutions is a well-proven automation kit for AGVs. The latest version (NDC8 3.0) with a new functionality lets the system find the best way for each AGV. Advanced algorithms thereby replace the need for manual traffic rule planning, saving time not only during start-up but also when making changes in the future.

“This new generation of software gives time savings of 40-50 percent,” says Rodrigo Alcaraz García-Tejedor, Robofast Application Manager at ASTI. “You don’t only save time when designing the system, you also save time once the commissioning has finished. Knowing that the system is intelligent means I don’t have to think about the traffic anymore.”

Towards the vision

Kollmorgen is working towards the vision of “design and commissioning in less than a day.” The previous step was the release of natural navigation, and the 3.0 version of NDC8 pushes the company even closer to realizing its vision.

You get the latest information on NDC8 3.0 by subscribing to this newsletter. If you are planning on buying AGVs, you can contact any of the companies participating in Kollmorgen’s partner program. Or contact us directly for more information.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…