Skip to main content
blog | Speed up your e-commerce with smart automation |
|
2 minute read

Speed up your e-commerce with smart automation

The Chinese e-commerce market is growing by two digits yearly. Impressive numbers paving the way for a prospering future, but also posing demands on delivery speed and quality. Automated Guided Vehicles (AGVs) such as carts and mobile robots, based on a proven platform, solve many intralogistics challenges thereby allowing profitable growth.

Automate to become profitable

Strong e-commerce growth encourages more and more companies to enter the market. This leads to a tight race where getting hold of the right competence and delivering undamaged products in time are crucial to success. Automation is often considered an alternative, but many automation solutions are fixed and simply don’t have the flexibility needed in this ever-changing world of e-commerce. On the other hand, automation is essential to meet all the staff and delivery challenges. Luckily, there is another alternative.

Accelerate your automation

The fast track to automation, and thereby to profitable e-commerce growth, is spelled vehicle automation. Using automated guided vehicles such as carts and mobile robots, you can be up and running with your automated system in just a few months and the payback period is often as low as 1-2 years. Compared with fixed automation, vehicle automation greatly increases efficiency without substantial investments.

Correctly managed, AGV installations can also raise the level of work satisfaction, making it easier for you to keep and train your staff. Which, in turn, opens up for improvements in delivery speed and quality.

Rely on a proven platform

When demand is high and time is tight, standardization is key to success. NDC Solutions is a standardized platform developed for customization of AGVs in all sorts of industries all over the world. All vehicles that perform intralogistics tasks such as picking and sorting can be connected and easily integrated with enterprise and warehouse management systems. With an installed base of more than 20,000 vehicles, NDC Solutions is the perfect platform for speeding up your e-commerce.

Feel free to contact us for further information, and don’t forget to check out our website for everything from inspiring articles to technical details.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…