Skip to main content
blog | Getting rid of bugs for good |
|
2 minute read

Getting rid of bugs for good

Automated tests of automated guided vehicles such as carts, mobile robots and tuggers. It might sound futuristic but is reality every day at Kollmorgen. Automated tests pave the way for continuous deliveries of new and updated applications without bugs. What used to take days to test is now down to hours.

New way of testing

Some years ago, Kollmorgen decided to start with automated testing. Improving quality assurance and cutting time to market for applications were the main reasons. A tough challenge as the product life cycles are 10 years and more. You need to make sure that all system software versions (17 at the moment) work on all computer platforms (16 at the moment).

“Automated tests give you the chance to test the same scenario again and again,” says Simon Bokesand, Chief Engineer in Software Quality Assurance at Kollmorgen. “That is impossible with manual tests. When you have written code for a certain test scenario, you can use it for all new releases of applications to prevent old bugs from coming back. Our vision is zero bugs.”

Driven by user needs

NDC Solutions is the name of the automation kit from Kollmorgen. The kit consists of hardware, software and navigation technologies. New types of automated guided vehicles (AGVs) are evolving all the time, and for end-users to survive in their markets, a higher degree of customization is needed. The answer from Kollmorgen is continuous deliveries of new and updated applications.

“Automated testing is crucial to cut lead times and improve quality,” says Simon. “We need to make sure that our partners get a toolbox from us that works. Their reputation is at stake, and they need to prove that they can live up to the new world of ever-increasing demands.”

With automated tests, it is also possible to test functionality and correct bugs at different places and in different time zones. The next day you as a test engineer walk into the office, your test results are ready.

Area of the future

Self-driving buses, cars and trucks are about to revolutionize daily life. Automated testing is fundamental to secure safe transportation in a society without drivers. Every little scenario of potential danger needs to be tested, and there is no chance of doing that manually.

Driverless vehicles in manufacturing plants and warehouses are nothing new. Kollmorgen has been in this market since the early 1970s. But now when Industry 4.0 is turning into a reality, manufacturing, warehousing and transportation are all linked together. Using automated tests for AGVs strengthens that part of the chain.

Our newsletter is also automated. Feel free to subscribe, and you will get the latest news about automated guided vehicles right into your inbox. You are always welcome to contact us or any of our partners.

Consult an Expert

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
The Future of NDC: Smarter Integration for AGVs and AMRs

The Future of NDC: Smarter Integration for AGVs and AMRs >

Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs

Kollmorgen Launches the new generation of AC and DC Motor Controllers for AGVs and AMRs >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…