Ana içeriğe atla

Search Articles

Archived G&L Technical ManualsThe following lists archived technical manuals for G&L products. For the most recent versions of these manuals visit G&L Technical Manuals İngilizce
G&L Technical ManualsThe following lists the most recent technical manuals. For archived versions of these manuals visit archived manuals İngilizce
Reading a Thermocouple in units of 0.1 Degrees C in a PxMM ProjectIn a KAS project, the following outlines reading a thermocouple temperature in units of 0.1 Degrees C from a AKT-AN-200 or AKT-AN-400 slice I/O module. İngilizce
KAS and Beckhoff stepper motor terminal EL7047A few simple steps to work the Beckhoff terminal EL7047 with KAS İngilizce
G&L Application NotesG&L Motion Control PiC Application Note Master List İngilizce
G & L CAD DrawingsA free DXF/DWG viewer, which allows printing CAD files, is available from SolidWorks.com. İngilizce
How do I insert PDO padding in the KAS PDO Editor?Some EtherCAT devices require padding data (empty data) inside their PDO content.  Some of these devices must have their PDO configuration entered or edited manually.  Here is an example of the PDO mapping for one of these devices as it shows up in another application’s PDO viewer: İngilizce
KAS Project File Clean-upIf the KAS project file size is unexpectedly too large, it is likely that there are some legacy or possibly corrupt HMI project files included in the project. To clean-up unnecessary and/or corrupt files, do the following: İngilizce
How can I access the HMI (AKI) service menu?The previous AKI-CDT-MOD-xxxx models have hardware switches to access the various modes and service menu.  This is documented in the installation manuals: İngilizce