Ana içeriğe atla

Search Articles

Cam Profile Creation from SD cardAttached is a demo program that contains two subprograms to import data from a file on a PDMM SD card, or export data from an array to the SD card. This data can then be used to build a cam profile in the program and update the motion on the slave axis while everything is running. İngilizce
6410 Screw Terminals - Torque RequirementsThe DC Power (2) and Motor Phases (J3) are connected by plug-in screw terminal type connectors. İngilizce
WorkBench Crash at Startup - Configuration file(s) corruptionIn some very rare cases, some of the WB configuration files may be corrupted and it will prevent WB to start. It may happen if your computer crashed, if WB crashed or was stopped using the Task Manager while writing one of these files. İngilizce
Heidenhain Endat 2.2/01 or Endat 2.2/22This question comes up quite a bit about the Heidenhain Endat  .  Saying Endat 2.2 is only half the story.  There is Endat 2.2/01 which is the analog version.  Endat 2.2/22 is the fully digital version.  Endat 2.2/01 and Endat 2.2/22 are fully backward compatible with End İngilizce
KBM(S) and TBM(S) Minimum Ambient Operating TemperatureThe minimum ambient operating temperature, for the KBM, KBMS, TBM, and TBMS series motors is -40 degrees C. İngilizce
Automation of the AKD Drive with a Siemens S7-1200 and S7-1500 PLC and Modbus TCPThe following utility provides a connection between AKD servo drive (other than the Profinet drive) and Siemens SIMATIC S7-1200/S7-1500 programmable logic controllers (PLC) using Modbus TCP programmed in TIA V13. İngilizce
Torque mode control of an axis with KAS ControllerThe attached demo project shows how to control a servo axis with a KAS controller in Torque Mode instead fo the default Position Mode. İngilizce
Writing Data to the PDMM SD Card or Embedded FlashThis application note describes the process of writing data to the SD card or the embedded flash on the PDMM in .CSV (comma separated variable) format.  This is a general overview for writing data.  More read/write functions can be found in the KAS help section under File Manage İngilizce
EMI ChecklistThis Application Note describes the various methods and combinations of methods for grounding and shielding. Following these recommendations will help minimize or eliminate problems encounters with electrical noise in your application. İngilizce