KAS Web Server - Overview
The KAS PxMM Controllers contain a built in webserver for access to the PxMM without having to work through the IDE. Functionality include:
- Starting and stopping a project
- Configuring a project to automatically start running the PxMM powers up
- Changing controller FW
- Geting PxMM diagnosis information
- Reading and/or retrieving data files
- Backing up and Restoring the PxMM
- Setting up a custom IP address
- Clearing Controller errors (faults)
- other
The following video goes through these features.
Home >
Knowledge Base >
FAQs >
Downloads >