Pular para o conteúdo principal

Search Articles

FAQ SeitenIm Folgenden finden Sie Links zu den verschiedenen FAQs (Frequently Asked Questions) auf dieser Website. alemão
Creating and Using a Recipe in KVB and AKI PanelA recipe can be used in an HMI program to store and select groups of data to be used without having to enter the data each time it is used.  It is easy to create a recipe in KVB by clicking on Insert / Recipe and give the recipe a name.  A recipe consists of Items and Data.  Each… inglês
Analog I/O Parameters - I/O Terminals for Variable MappingThe following link points to an example from the KAS Online Help which discusses process data transferred to the Bus Coupler for variable mapping. inglês
EtherCAT Scan & Association - Adding Physical I/O SlicesThe following link points to an example from the KAS Online Help which shows how to add a physical I/O slice to an existing project. inglês
EtherCAT Scan & Association - Couplers & I/O SlicesThe following page is an example from the KAS Online Help which shows how to add a coupler to an existing project. inglês
EtherCAT Coupler Error Handling And DiagnosisThe KAS IDE help has an extensive section on EtherCAT error handling.  inglês
KAS Support of AKT-SM-Lxx Stepper SlicesA topic from the KAS Online Help which discusses the support of AKD-SM-Lxx stepper slices by KAS. KAS Support of AKT-SM-Lxx Stepper Slices inglês
Using Homing Mode 17 With Single-turn and Multi-turn feedback TypesThis application note covers Homing Mode 17 in the AKD drive, how it works, and how to use it. inglês
IDC EC Series "Brake on Screw" OptionReplacement cable part number: 550-004  inglês