AKD Profinet Fieldbus Support Landing PageThis page provides links to Sample Projects, Training Materials, and Application Notes & Articles related to Profinet on AKD drives.
WorkBench LoggingDebugging interaction problem between WorkBench and drives may be facilitated by using the built-in logging mechanism.
inglês
Sample Projects for Siemens S7-1200 / S7-1500 PLC's and the AKD Profinet DriveThis page provides information and downloads related to TIA Portal sample projects for Profinet communication between the Siemens S7 PLC's and AKD Profinet drive.
The sample projects use a function block to handle the telegram data and state machine (Control Word and Status Word).…
inglês
Getting Started with a KAS IDE Project Template The following video details how to get started with the KAS IDE (Integrated Development Environment) that is used to create PxMM controller application software. It includes:
Open and use a Getting Started Template Project
Overview of the sections in a project
Review of the…
inglês
KCM and FusingIt's not listed in the manual but all KCM modules have the necessary fusing built in. Not field replaceable because, if the fuse is blown, the unit will need to be repaired.
inglês
KAS ST (Stuctured Text) EditorThis video introduces the KAS IDE, ST (Structured Text) Editor
Loading...
Covered in the Video:
Syntax
Compile, run, and animation
Comments
Using Function and Function Blocks
Conditional Statements
Shortcut keys
(Reference to) Debugging