Pular para o conteúdo principal

Search Articles

KAS Training Videos - Controller Application Software DevelopmentTo help get started developing an application with the controllers, training videos are now available on the KAS-IDE (Integrated Development Environment). inglês
KVB Release NotesRelease Notes inglês
DC Torquer Old CatalogOld DC Torquer Catalog for NT, QT, and T inglês
PCMM Dual-Core - New KAS Controller Model!The PCMM (Programmable Controller Multi-Axis Master) Dual-Core is a PCMM 1.2GHz with two CPU cores. It shares the same electronic hardware, connectors, and signals as the PCMM single core model. It has the same features, functionality, memory, and flash storage as the PCMM single core model. inglês
EOT (End of Travel) Software Position Limits in a KAS applicationIn a KAS PxMM application program, to setup software End Of Travel (EOT) position limits: inglês
HOME.MODE 0 vs. HOME.SETHOME.SET When HOME.SET when executed it will set the commanded and current position equal ( PL.CMD an PL.FB respectively )  to the HOME.P value. HOME.P can be set by the Workbench Terminal, on the home screen in the “Position” field ( see below ) or over fieldbus if desired. inglês
KAS v3.0 Software is Now Available!New Features AKD2G Drive Integration: Single and Multi-Axis drive variants Features not yet available: firmware download, capture, I/O, feedback #2-5 Note: Please contact Kollmorgen for latest AKD2G firmware and KAS software. inglês
Shared Drive in PDMM or PCMM Application Fails to MountThe PxMM can work with data from an external or shared drive. Mounting is the software process in the PxMM that enables it to read and write data to/from a shared drive. If the mounting process fails in the PxMM the following message will appear in the IDE Controller Message Log. inglês
Can an AKD EtherNet/IP drive operate using a different command source other than Service?We are often asked if an AKD-P-NBEI ( EtherNet/IP ) drive can use step/dir (electronic gearing ) or analog as the command source and simply use EtherNet/IP for inglês