CoggingGeneral
Cogging torque designates a phenomenon with electrical motors, which possess permanent magnets in the stator and a slotted anchor from electric sheets or a slotted stand and an anchor with permanent magnets.
inglês
HiperFaceHIPERFACE®
The High Performance Interface is the standard interface for SICK-STEGMANN motor feedback systems.This interface was specially developed for the requirements of digital drive control and offers the user standardised and simplified mechanical and electrical interface
inglês
EthernetGeneral
Ethernet is a cable based data network technology for local data networks (LANs). It enables data exchange in the form of data frameworks between all attached devices in a local area network (LAN) (computers, printers and similar).
inglês
SSIThe Synchronous Serial Interface (SSI) is an interface for absolute angle encoders (position encoders). You receive an absolute position information via a serial data transmission. The SSI interface has been developed by Max Stegmann GmbH and is used today by several manufacturers.
inglês
Step Direction InterfaceYou can connect the servo amplifier to a third-party stepper- motor controller. The servo motor follows the step-direction signals of the stepper controller.
inglês
GrayCodeThe Gray Code (named after the physician Frank Gray) is a symmetrical procedure to generate a code, where neighbor numbers differ in one bit only. This reduces the maximum possible error when transferring an analog signal to a digital code.
inglês
Modbus Bus
The Modbus protocol is a communications protocol that is based on a client-server architecture. It was created in 1979. In the industry, the Modbus has developed into a de facto standard since it is an open protocol.