Step Direction Interface
You can connect the servo amplifier to a third-party stepper- motor controller. The servo motor follows the step-direction signals of the stepper controller.
Parameter setting for the servo amplifier is carried out with the aid of the setup software (electronic gearing). The number of steps can be adjusted, so that the servo amplifier can be adapted to match the step-direction signals of any stepper controller. Various monitoring signals can be generated.

Home >
Knowledge Base >
FAQs >
Downloads >