AKM Motor Set up for SC900An AKM motor with resolver can be operated with an SC900 series amplifier providing that the motor is within the current limitations of the drive. Typically the motor resolver offset must be set to 240. This is in the configuration screen and called COMMOFF.
AKD Spring Clamp ConnectorsAll Revision 9 and almost all Revision 7 AKD Control boards use Amphenol 3.5mm connectors for X7 and X8.
Both the header and the mating connector are bespoke items from Amphenol. Phoenix numbers for spring clamp connectors are:
AKD Maximum Commutation FrequencyMaximum FW commanded speed is 15,000 RPM.
Maximum commutation frequency is set by PWM frequency and/or position feedback device sampling frequency.
inglês
Insulation MaterialInsulation material typically depends upon the application. For example, environmental conditions such as temperature, chemical exposure, and abrasion/tear resistance should all be considered when choosing an insulation material.
inglês
BiSSThe bidirectional digital sensor interface (BiSS) safeguards the communication between position encoder and servo amplifier and can transfer measurements of up to 8 sensors simultaneously.
inglês
Motor Data Legend
Symbol
Dimension
English
Description
M0
Nm
Standstill torque
The standstill
inglês
FusesRequirements to fusing of lines and devices are different for CE and UL/cUL regions.