AKD2G Gantry Application SetupA gantry system consists of two motors sharing a load with minimal wasted energy used in opposing each other. This document is an attempt to help with setup and use of the Kollmorgen gantry control embedded in the AKD2G two-axis drive. For the scope of this document, I will refer to the…
Coupler Sizing - AKT2G Remote IOThe AKD-PDMM controller/drive, PCMM standalone controller, AKD, AKD2G, and S700 drives all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first before…
Configuring BBH SCU with AKD2G SRA parameters This article shows how to make a simple safety Application with KAS and SafePLC2.
The Functional Safety parameters can be configured in WorkBench or in the BBH SafePLC2. Both methods are described here.
AKD and the Raspberry PiRaspberry Pi Foundation and its background.
The foundation's goal was to advance the Computer Science, Programming, and engineering education of children and adults with a low-cost and high-performance solution.
From Raspberry Pi Foundation itself:
inglês
Configuring The AKD X9 EEO AS General Digital I/OThe X9 Port on the AKD drive is generally used as an encoder input, EEO (encoder emulated output), or not used. However, the AKD also has the feature to use the X9 port as general I/O.
inglês
S300, S700 ROFFSABS, Absolute Encoder Single TurnWhen configuring the S700 or S300, homing with an absolute encoder you will need to use ROFFSABS. ROFFSABS provides the necessary offset when physically homing. Single Turn Absolute is absolute to 1 rotation of the motor.