Skip to main content

As populations grow, societies develop, and new diseases like COVID-19 emerge, the ability to quickly ramp up vaccine development and production is critical. Public health can’t wait.

In the fluid-handling pumps of vaccine-production equipment, motion systems must ensure the utmost precision. They must be able to withstand extreme environments and rigorous cleaning protocols. They must perfectly fit the system’s unique requirements for torque, power, feedback, sizing, mounting and cabling—often requiring a high level of customization. Yet these systems must be available with a reliable supply, in the quantities needed, wherever vaccines are produced.

Our 2G Motion System provides perfectly matched servo drives and motors that significantly reduce space requirements with no compromise to performance. Our rugged, stainless steel AKMH series servo motors are designed to perform flawlessly despite the frequent, harsh cleaning routines required to maintain a hygienic clean-room environment. Kollmorgen Powermax NEMA 23 stepper motors deliver precise motion control without the need for encoders and feedback circuits, and they feature oversized bearings for increased service life.

Request a Quote Why Kollmorgen?

Top Products for Vaccine Production

High TorquePOWERMAX II® M and P Stepper Motors - Kollmorgen

POWERMAX II® M and P Stepper Motors >

The POWERMAX II® M and P Series are NEMA 23 stepper motors feature an octagonal housing and are available in half-, single-, and two-stack configurations. These units offer a wide variety of standard options and affordable co-engineered modifications, without sacrificing scalability and lead time.

AKM Motors >

Our best-in-class, high-performance servomotors offer a wide range of mounting, connectivity, feedback and other options. More than 500,000 standard models are available along with co-engineered modifications to suit almost any application…
Stainless Steel AKMH Series

Stainless Steel Food Grade AKMH Series >

The AKMH Series is built to withstand the most rigorous of washdown regimens. The combination of the AKMH’s IP69K construction and corrosion resistant materials make for a servo motor that will last the life of your machine.
2G Motion System

2G Motion System >

Kollmorgen introduces the next generation of motion for more ambitious machines built on more capable performance and more confident engineering. The Kollmorgen 2G Motion System harnesses the full performance potential of our leading AKM2G servo motors and perfectly matched AKD2G drives designed to deliver unrivaled power density and control. The result is significantly enhanced torque, responsiveness and SafeMotion capabilities in a compact footprint that enables easy installation and total flexibility.

Related Resources

Rapid Scale-Up of Blood Gas Analyzer Production, Kollmorgen

Rapid Scale-Up of Blood Gas Analyzer Production >

The COVID-19 pandemic has created a massive spike in the demand for medical equipment in every region of the world, including personal protective equipment, laboratory test systems, ventilators and more. A major global supplier of blood gas analyzers…
Rapidly Scaling Production of Critical Equipment, Kollmorgen

Rapidly Scaling Production of Critical Equipment >

In the fight against COVID-19, the soaring demand for face masks has led to a severe undersupply.  Beckmann Automation GmbH, a German machine builder that has traditionally manufactured machines for mattress and belt production, quickly stepped…
Kollmorgen Helps Rapidly Scale CT Scanner Production, Kollmorgen

Reliable and Consistent Supply of Motion Systems >

When the world became aware of the COVID-19 outbreak first identified in Wuhan, China, it quickly became clear that greatly increased diagnostic capacity would be needed. Early in the outbreak, one of the world’s largest producers of diagnostic…