Skip to main content
Success Story | 2 minute read

Rapidly Scaling Production of Critical Equipment

Kollmorgen Motion System Enables Quick Response to COVID-19

Challenge

In the fight against COVID-19, the soaring demand for face masks has led to a severe undersupply. Driven by market demand and requests from governmental bodies, many companies have shifted their typical production focus and retooled to produce this essential personal protective equipment. Beckmann Automation GmbH, a German machine builder that has traditionally manufactured machines for mattress and belt production, quickly stepped in to meet this urgent need.

Beckmann’s primary challenge has been an extremely short timeframe for designing and building new face mask production equipment coupled with the challenges of working under COVID-19 restrictions. To streamline the design of its new machine, Beckmann has sought partners able to provide complete subsystems, rather than individual components, in order to significantly reduce the number of integration points and accelerate speed to market.

These considerations are particularly important with regard to the new machine’s motion system: the motor, gearbox, drive and cable. Beckmann chose to significantly speed design and production while reducing risk by sourcing the motion system from a trusted partner who has already confirmed the required performance and can ensure a reliable supply of all elements.

Solution

Based on many years of close collaboration, Beckmann chose Kollmorgen as its motion partner for the new breathing mask machine. Kollmorgen is providing a motion subsystem consisting of an AKM servo motor mounted with a gearbox, an AKD servo drive and a single power/feedback cable—all perfectly matched to ensure optimal performance.

This subsystem has already been proven to offer multiple advantages in other Beckmann machines. First and foremost, the servo system delivers the high performance that Beckmann needs to consistently exceed its customers’ expectations and outperform the market. Second, Kollmorgen’s single-cable and SFD (smart feedback device), optimized for the AKD drive, enables Beckmann’s customers to quickly set up the whole system, saving a tremendous amount of time.

Time to market for face mask production was especially critical. To help Beckmann meet the need, Kollmorgen mobilized a large cross-functional team encompassing sales, applications support, production operations, supply chain and customer service. This team quickly identified the appropriate motion solution and has ensured that the supply of each subsystem component is synchronized and meets Beckmann’s lead time requirements.

Results

An integrated motion solution from a single partner eliminated the performance risks, coordination difficulties and delivery uncertainties that are practically inevitable when working with multiple suppliers. Kollmorgen’s cross-functional team reduced the normal delivery time for a full motion sub-system design by 70%. This quick response has helped Beckmann deliver machines to their customers in the shortest possible time.

  • The motion system and support from Kollmorgen enabled Beckmann to ship their first batch of machines within 6 weeks from design.
  • Beckmann successfully transitioned into a completely new market segment, from which they are expecting to generate incremental sales in the years to come.
  • The new Beckmann machine offers breathing mask producers ultimate flexibility. Its modular design enables easy and quick shifts from partial to full automation, the addition of packing stations, and the ability to change over from production of masks to filters and other textile products for a range of applications.
  • Powered by the Kollmorgen subsystem, the face mask production line is able to produce 70 parts per minute, and up to 100,000 parts per day.

Kollmorgen has also supported a similar accelerated production schedule for a number of other key medical device manufacturers worldwide who provide CT scanners for both hospitals and mobile care

“Kollmorgen is our longstanding and trusted partner for motion. Kollmorgen’s timely and effective support for our mask production line helped us navigate through these challenging times and meet even the toughest turnaround time commitments with our customers” - Kevin Beckmann, Sales Manager, Beckmann

Learn More

Ready to design and build a more ambitious machine?

Learn more Talk to a Motion Expert Explore Our Design Tools

 

About Kollmorgen

Kollmorgen has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, linear actuators, gearheads, AGV control solutions and automation platforms. We deliver breakthrough solutions that are unmatched in performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Advanced Surgical Robots: Designing Compact, Powerful Motion for the Next Generation

Learn the key criteria for designing axially compact arm joints that minimize space, maximize torque, and deliver precision performance in surgical robots.
Learn More

Build a Better Patient Experience Into Your Imaging Device

Every radiology department wants to deliver the highest-quality diagnoses to support the highest-quality patient care. The key to improving the patient experience is precise motion under perfect control. That’s Kollmorgen’s specialty.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite

Mastering Motion: A Comprehensive Tour of the Modern Surgical Robot Suite >

Step into the future of surgical robotics and enhance your understanding of what’s possible. This webinar offers a detailed exploration of the cutting-edge components that drive precision and efficiency in today's advanced surgical robots.
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Kollmorgen Motors for Medical Imaging: Proven Processes, Reliable Delivery >

Few business challenges are as formidable as designing, manufacturing and delivering medical imaging equipment to healthcare organizations around the world. From mechanical and electrical components, to communication and control systems, to motion…

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Kollmorgen Azure Surgical Robotics Story

Enabling New Surgical Possibilities with High-Torque, Low-Temperature and Compact-Size Motors >

A new collaborative surgical robot helps surgeons do their best work, in more types of surgery, delivering better outcomes. TBM2G servo motors make it possible.
Surgical robotic arms in operating room.

Advanced Surgical Robots: Designing Compact, Powerful Motion for the Next Generation >

Learn the key criteria for designing axially compact arm joints that minimize space, maximize torque, and deliver precision performance in surgical robots.

Surgical Robotics Process & Delivery >

Discover all the solutions Kollmorgen offers for robotic surgery systems, from the surgeon’s console to the patient table to next-generation robotic arms. 
Kollmorgen Motion for Mammography

Kollmorgen Motion for Mammography >

Whether fixed or mobile, whether 2D or 3D, whether targeted to major providers or remote clinics—a successful mammography machine must meet specialized requirements.
Co-Engineer Superior Medical Motion in 5 Simple Steps

Co-Engineer Superior Medical Motion in 5 Simple Steps >

Kollmorgen co-engineering is a partnership for the success of your imager, from specifying the motion system requirements through meeting regional EMC compliance requirements and delivering the products and local engineering assistance and technical…