Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen
See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.
One Site, Two Fleets, VDA 5050 in the Middle: Jungheinrich’s tailored AGV system meets Wildeboer’s long-term needs
Jungheinrich’s tailored AGV system meets Wildeboer’s long-term needs
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations
DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully implemented Jungheinrich Automated Guided Vehicles (AGVs) with Kollmorgen technology and is the first terminal within DB Schenker land to use automated…
Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla
Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow aisle automated guided vehicles (VNA AGVs), each equipped with Kollmorgen technology.
AGV car parking robots
Yeefung, an AGV partner to Kollmorgen, has developed a new generation of their car parking robot.
High Reach AGV in Solar Panel Manufacturing
Seraphim Solar System have improved accuracy and efficiency in their warehouse by introducing AGVs.
High Reach AGV in 3PL warehouse
By using high-reach AGVs, Ocean East International Logistics decrease their operational cost.
Mobile Robots for Hospitals
The AGV System at Herlev Hospital in Denmark use Natural Navigation.
Smart Mobile Robots at Philips
Asti has implemented an AGV system for Philips, that uses Kollmorgen’s next generation technology.