Skip to main content

Kollmorgen Support Network

KAS Associated Firmware By Release | 30 Apr 2019 | |

KAS Associated Firmware By Release

The following table provides a resource for what firmware is associated with each release of the KAS IDE. This includes both firmware for the drive built into the AKD-PDMM controller, as well as the firmware for other drives that may be used within KAS.

Version Description Type Name
3.01 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-18-00-004
Resident r_00-00-63-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-18-00-004)
1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-18-00-004)
AKD Drive Firmware AKD-N akd-n-xxEC-01-18-00-004.i00
AKD-P akd-p-NBxC-01-18-00-004.i00
AKD2G Drive Firmware AKD2G-SPE akd2g-spe-a-02-00-00-000.i00
3.00 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-17-00-000
Resident r_00-00-60-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-17-00-000)
1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-17-00-000)
AKD Drive Firmware AKD-N akd-n-xxEC-01-17-00-000.i00
AKD-P akd-p-NBxC-01-17-00-000.i00
2.12 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-16-00-002
  Resident r_00-00-56-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-16-00-002)
  1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-16-00-002)
AKD Drive Firmware AKD-N akd-n-xxEC-01-16-00-002.i00
  AKD-P akd-p-NBxC-01-16-00-002.i00
2.11 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-15-00-001
  Resident r_00-00-55-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-15-00-001)
  1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-15-00-001)
AKD Drive Firmware AKD-N akd-n-xxEC-01-15-00-001.i00
  AKD-P up to r.8 akd-p-NACC-01-15-00-001.i00
    akd-p-NAEC-01-15-00-001.i00
  AKD-P r.9 akd-p-NBCC-01-15-00-001.i00
    akd-p-NBEC-01-15-00-001.i00
2.10 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-14-00-003
  Resident r_00-00-54-000.i00
  Resident for AKD-C/N r_00-00-55-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-14-00-002)
  1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-14-00-002)
AKD Drive Firmware AKD-C akd-C-CBEC-01-14-00-003.i00
  AKD-N akd-n-xxEC-01-14-00-003.i00
  AKD-P up to r.8 akd-p-NACC-01-14-00-003.i00
    akd-p-NAEC-01-14-00-003.i00
  AKD-P r.9 akd-p-NBCC-01-14-00-003.i00
    akd-p-NBEC-01-14-00-003.i00
2.09 AKD Firmware for KAS Operational AKD-Firmware-for-KAS-V01-13-00-004
  Resident r_00-00-47-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-MCEC-01-13-00-004)
  1.2 GHz AKD PDMM AKD PDMM Servo Drive Firmware (AKD-M-M1EC-01-13-00-004)
AKD Drive Firmware AKD-P up to r.8 akd-p-NACC-01-13-00-004.i00
    akd-p-NAEC-01-13-00-004.i00
  AKD-P r.9 akd-p-NBCC-01-13-00-004.i00
    akd-p-NBEC-01-13-00-004.i00
2.08 AKD Firmware for KAS Operational  
  Resident r_00-00-40-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM servo drive firmware akd-m-mcec-01-10-00-003.i00
AKD Drive Firmware AKD-P up to r.8 akd-p-NAEC-01-10-00-003.i00
  AKD-P r.9 akd-p-NBCC-01-10-00-003.i00
2.07 AKD Firmware for KAS Operational  
  Resident r_00-00-40-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM servo drive firmware akd-m-mcec-01-10-00-003.i00
AKD Drive Firmware AKD-P up to r.8 akd-p-NAEC-01-10-00-003.i00
  AKD-P r.9 akd-p-NBCC-01-10-00-003.i00
2.06 AKD Firmware for KAS Operational  
  Resident r_00-00-40-000.i00
Firmware for the drive built into device 800 MHz AKD PDMM AKD PDMM servo drive firmware akd-m-mcec-01-08-00-003.i00
AKD Drive Firmware AKD-P up to r.8 akd-p-NAEC-01-08-00-003.i00
  AKD-P r.9 akd-p-NBCC-01-08-00-003.i00

About this Article

Will Gaffga