The AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier).
The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of…
The following table provides a resource for what firmware is associated with each release of the KAS IDE. This includes both firmware for the drive built into the AKD-PDMM controller, as well as the firmware for other drives that may be used within…
We have enhanced our new firmware 6.05 for S700 and S300 to now support the latest AKM2G servo motor family via plug and play. The motor database in the servo amplifier and in the DriveGUI now support AKM2G.
For space reasons, however, we had to…
Firmware on an AKI-CDB Panel can be loaded either by Ethernet or by USB.
Setup if Loading via Ethernet
If loading via Ethernet, make sure that the computer IP address is in the same range as the AKI - CDB Panel and that the subnet mask is the…
This FAQ helps you understand AKD backup FPGA firmware, a situation where the motor holding brake can unintentionally disengage, whether your hardware could be affected, and how to remedy the situation.