Servo Motors
The servo motor is an engine, that can drive to different set point positions and then maintains these in the sense of a control drive. The position is thereby in case of a rotatory engine a angle position and in the case of a linear motor a distance position. Starting and maintaining the…
Motor ChokeWhy use motor chokes? The motor choke: compensates high capacitive charge/discharge currents typical of shielded motor cables approx. 25 m and longer; reduces current alternation noise in the motor; reduces current ripple in the motor. Read more.
inglês
AKD PDMM LED DisplayValid for AKD-M (AKD PDMM)
The AKD PDMM Drives have a two digit plus a one digit display on the front. Status, faults and warnings are shown there.
MultiFieldbusMulti-Fieldbus is the ability of Kollmorgen servo amplifiers to communicate with a lot of different fieldbus systems. These bus systems are accessible either with option cards, firmware variants or device variants.
inglês
REACH RegulationThe European REACH regulation (Registration, Evaluation, Authorisation and Restriction of Chemicals) No 1907/2006, has been introduced on June 1st, 2007, transitional period 1 year.