Salta al contenuto principale

Kollmorgen Support Network

Search Articles

Delay of Enable SignalValid for S300, S700 Inglese
Analog Position SetpointValid for S400, S600 The analog input can be used for the setting of the position from firmware version 3.10. The function is similar to a master/slave effect. Inglese
Speed adjustment with external position feedbackValid for S300, S400, S600, S700 Inglese
Memory CardValid for S700 Inglese
Reaction to fault situations S300-S700Valid for S300, S700 Depending on the current trouble, faults are managed differently (different error levels): Inglese
Setup of Acceleration Profile TablesValid for S300, S400, S600, S700 Create table with Excel, normalize current / position values   Inglese
Analog Torque LoopValid for S400, S600 Inglese
Safe Reduced SpeedValid for S400, S600 Inglese
Motion Task SeriesValid for S300, S400, S600, S700 Inglese