Salta al contenuto principale

Kollmorgen Support Network

Search Articles

BiSSThe bidirectional digital sensor interface (BiSS) safeguards the communication between position encoder and servo amplifier and can transfer measurements of up to 8 sensors simultaneously. Inglese
Motor Data Legend Symbol Dimension English Description M0 Nm Standstill torque The standstill Inglese
FusesRequirements to fusing of lines and devices are different for CE and UL/cUL regions. Inglese
CoggingGeneral Cogging torque designates a phenomenon with electrical motors, which possess permanent magnets in the stator and a slotted anchor from electric sheets or a slotted stand and an anchor with permanent magnets. Inglese
HiperFaceHIPERFACE® The High Performance Interface is the standard interface for SICK-STEGMANN motor feedback systems.This interface was specially developed for the requirements of digital drive control and offers the user standardised and simplified mechanical and electrical interface Inglese
EthernetGeneral Ethernet is a cable based data network technology for local data networks (LANs). It enables data exchange in the form of data frameworks between all attached devices in a local area network (LAN) (computers, printers and similar). Inglese
SSIThe Synchronous Serial Interface (SSI) is an interface for absolute angle encoders (position encoders). You receive an absolute position information via a serial data transmission. The SSI interface has been developed by Max Stegmann GmbH and is used today by several manufacturers. Inglese
Step Direction InterfaceYou can connect the servo amplifier to a third-party stepper- motor controller. The servo motor follows the step-direction signals of the stepper controller. Inglese
GrayCodeThe Gray Code (named after the physician Frank Gray) is a symmetrical procedure to generate a code, where neighbor numbers differ in one bit only. This reduces the maximum possible error when transferring an analog signal to a digital code. Inglese