Salta al contenuto principale

Kollmorgen Support Network

Search Articles

Single Phase OperationValid for S300 Usage of full controller current at reduced DC link voltage. Inglese
Fault Codes Amplifiers Electronics EA control circuitry EL logic inputs/outputs EV Inglese
Fault Codes Motors Motors Mechanical / motors Other MA motor Inglese
Fault CodesDevices that have been sent to Kollmorgen Europe GmbH for repair are examined and the result of the examination are documented in a report. The fault codes, which are used in these reports are explained in seperate tables for Motors and Amplifiers. Inglese
Flash Option CardValid for S600 with FW 5.70 ...5.99, 7.xx Inglese
SSI Encoder EvaluationValid for S300, S700 from FW 2.14 Parameter setup for SSI Encoder evaluation A SSI encoder (absolute encoder) must be setup with these parameters: Inglese
Servostar Links Abbreviations Country Codes Language Codes Mul Inglese