Salta al contenuto principale

Kollmorgen Support Network

Search Articles

Servodisc Brush Replacement CommentsUnlike our other brush motor products, Kollmorgen does not sell replacement brushes for our Servodisc motors. Inglese
AKM Motor Shaft Seals (Teflon & Viton)This gives a brief overview of the teflon and viton shaft seals for the AKM product line.  The attachment contains the text listed in the below as well as some pictures of installed seals and 2D outlines of the seals. Inglese
Radford (R03) to Germany (D01) Accessories Cross ReferenceThis excel file contains many of the accessories sold in the U.S. and Europe.  Often the U.S. part number will coincide with the European standard of DE-XXXXX.  This file contains the part numbers that diverge from this standard. Inglese
Decentralized Drive SystemThe AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. Inglese
Coil Thermal Constant (MOTOR.CTF0)Calculating the coil thermal time constant for a motor based on the bulk motor thermal time constant. Inglese
Max Input Frequency for Aux Feedback J14 on S200 SynqNet The SynqNet option card J14 Aux feedback spec for A quad B digital incremental is 3 MHz line or 12 MHz count.For the 1 Vp-p analog sin-cos input max recommended Sin-Cos frequency is 625 kHz, although it can be usable up to an absolute max of about 1.5 MHz.  Inglese
AKD Command Source for ProfinetThe correct command source to use for AKD Profinet communication depends on the operation mode (or telegram) that is being used.  The command source will be set automatically by the drive based on which telegram has been selected. Inglese
AKD Single Phase Supply OperationOver the years, Kollmorgen has offered 120V/230V drives that can operate on a single phase AC supply.  Most of these are for laboratory or college applications.  In some cases, these applications experience under voltage faults or bus capacitor over loa Inglese
Starting Direction of AC Synchronous Stepper MotorThe AC Synchronous stepping motor may initially start in the opposite direction from the one desired. Inglese