Passer au contenu principal

Permanent Magnet DC Motor Catalog >

Why have design engineers depended on Kollmorgen permanent magnet DC motors for nearly 50 years? Value and Performance. Rugged, quality construction, backed by a 2 year warranty.

Aerospace & Defense Solutions >

The Aerospace and Defense industry has inspired innovation after innovation in the quest for an edge in operations, as well as in security and information exchange. Kollmorgen’s reputation for excellence and rapid development has led to a range of…

Robotic Solutions Brochure >

Our reputation for enabling robotic innovation continues to grow as Kollmorgen motors deliver motion to new robotic applications every year.

Electro-Optical / IR Stabilized Platform Motors Application Overview >

When the mission is critical, aerospace and defense contractors trust high-performance motion solutions from Kollmorgen to get the job done right

Kollmorgen Corporate Brochure >

A modern business with a rich history, Kollmorgen is a leading global provider of precision motion systems and components for OEMs that has been active in the industry for over a hundred years.

Direct Drive DC Torque Motors Brochure >

The Direct Drive DC Torque motor is a servo actuator which can be directly attached to the load it drives. It has a permanent magnet (PM) field and a wound armature which act together to convert electrical power to torque. This torque can then be…

Kollmorgen PMX Series Stepper Motor Catalog >

Kollmorgen’s stepper motors are designed with versatility, ease–of–use, and cost-effectiveness in mind. They provide high torque in a small package and come in a wide range of standard sizes, constructions, windings and options.

Kollmorgen Housed DDR Motors Catalog >

Catalog for Kollmorgen Housed direct drive (DDR) rotary motors

Kollmorgen KBM Series Brushless Motors Catalog >

Catalog for the Kollmorgen KBM series brushless motors. From the motor kit directly to the motion solution.

Kollmorgen Direct Drive Linear Motor Catalog >

Catalog for Kollmorgen direct drive linear motors

AKMH Stainless Steel Washdown Motor Catalog >

Designed for Fast Cleaning and Increased Uptime. The AKMH stainless steel motor is designed to meet the standards for IP69K, EHEDG, and 3A and is built with FDA approved, food-grade materials.