The 2G Motion System consisting of next generation motors, drives, and cable systems offer superior motion to deliver power and torque density at a significantly smaller size. From direct drive rotary and linear to housed and frameless, our cutting machine servo motors can handle every cutting technology, application and operating environment. And with gantry functionality, our 2G Motion System enables machine builders to achieve that next level of motion performance by tightly synchronizing two axes at the firmware level. This magnitude is typically faster compared to fieldbus update rates.
Cutting machines use lasers, plasma and waterjet to make highly precise cuts with speed and efficiency. Kollmorgen’s motors have the torque and power density needed to minimize payload inertia and maximize control for faster, more precise cutting. With motion performance designed and tuned to the specific task, we can integrate the right motor for each individual machine to offer you better performance at higher speeds.
Performance Starts with Kollmorgen Drives & Motors

Tips for Designing Next-Generation Performance
Cutting machine performance starts with high-quality products. It’s perfected with motors and drives customized to your application. Are you looking to design lighter, more efficient machines that use fewer and smaller parts? This white paper covers the five key areas that need to be addressed when optimizing your motion system.
Get the Right Tools to Speed Your Design
Having the right tools at your fingertips to empower you to assess what motor is right for you can help speed your design phase. Kollmorgen’s self-guided design tools help you model, choose and optimize products online, when you want and where you want.

Top Products for Laser, Waterjet and Plasma Cutters
Related Resources
High Definition Cutting: The Kollmorgen Advantage >
Plasma, laser and waterjet cutting machines can have very different applications, but they all have one thing in common, they depend on precisely controlled motion. To achieve next-generation accuracy, efficiency and productivity, machine builders…
Material Forming Overview Brochure >
Advanced material forming processes are defined by quality, repeatability and throughput. These requirements place unique demands on the performance of the motion systems that drive cutting, bending, braking and other material forming machines.
Automating Metal Forming Systems to Improve Productivity and Flexibility >
Learn how a major supplier of automated tube-cutting machines used direct-drive technology to transform metal-forming performance, precision and versatility. Get the details, and envision the possibilities for your own metal-cutting machine.
Better Cut Quality Through Improved Connectivity >
A Turkish-based company was looking to improve the cost, cut quality and machine serviceability of their flagship plasma cutting machine. Kollmorgen engineers implemented an AKM/AKD system solution to provide faster indexing and settle times. By…
Optimizing Laser Cutting >
Since 1992, an Italian-based company has specialized in the design and manufacture of laser machine systems that are used around the world to cut a variety of materials, including metal, wood, plastic, ceramic, glass, methacrylate and composite…
Simplified Controller Integration Speeds Time-to-Market >
The market for plasma cutting machines in North America is highly competitive, with customers looking for a variety of solutions—from big machines with high capacity and throughput to smaller machines for fabrication shops with more limited…
Taking Laser Cutting Performance to the Next Level by Enhancing Precision while Reducing Size, Weight & Cost >
Discover the motion technologies that enable next-generation laser-cutting system performance. Read the details in our case study, “Enhancing Precision While Reducing Size, Weight and Cost,” then envision the possibilities for your own metal-cutting…
Five Motion Tips for Optimal High-Definition Metal Cutting Performance >
Achieve next-generation performance for laser, waterjet and plasma metal-cutting machines. Optimize the fieldbus, control loop bandwidth, servo motor design, feedback system and cabling using these 5 motion tips for high-precision metal cutting.