Skip to main content

5 Considerations to Optimize Frameless Motors in Aerospace & Defense Applications

From design through deployment, a successful aerospace and defense program depends on efficient prototyping, cost-effective production and reliable supply. For these reasons, engineers prefer to specify motors that are readily available and affordable. Yet commercial off-the-shelf motors may not always meet the demands of stabilized platforms and actuators that must perform flawlessly under the most extreme conditions.

Higher shock loads. Optimized motor windings. A larger through-bore aspect ratio. How do you achieve these and other specialized motor attributes on a rapid development schedule, with assurance of meeting cost and supply requirements for a program that may be in service for decades?

Download as PDF

Fill out this short form

to view this Document

-OR-

Login / Register

to gain access to Kollmorgen content

Privacy Statement - By sending us your contact details you agree that your personal data/user behavior can be electronically stored and processed. If you no longer wish to receive the enewsletter, you can unsubscribe at any time.

CAPTCHA

Motion for Missiles: Optimizing Performance

Missile systems continue to evolve to meet specialized needs — from tactical guided missiles to longer-range strategic weapons, each designed for launch from a particular platform to reach a particular target. Defense contractors are under pressure to design and produce ever more sophisticated systems in greater quantities to meet today’s national and global security needs.
Learn More

Electro Optic Infrared Systems

Electro-Optical/Infrared systems require smooth, responsive motion perfectly coordinated between azimuth and elevation axes. To acquire and hold a steady image, motion systems must endure and counteract forces such as the pounding of land vehicles in action, the turbulence of aircraft in flight, and the extreme conditions encountered at sea or even in space.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Enhance Missile Development with Advanced Motion Design

Enhance Missile Development with Advanced Motion Design >

This webinar will discuss the critical motion control elements needed for effective missile development and how these elements can work effectively together — from motors of all sizes to ball screws, resolvers, brakes, bearings and seals, to…

Motion for Missiles: From Speed of Innovation to Speed of Production  >

With rapid growth in the worldwide market for missiles, and demand for ever more innovative capabilities, engineers need rapid access to highly specialized motion systems, produced in reliable quantities. Learn how to greatly accelerate design and…

Motion for Missiles: Optimizing Performance  >

Missile systems continue to evolve to meet specialized needs — from tactical guided missiles to longer-range strategic weapons, each designed for launch from a particular platform to reach a particular target. Defense contractors are under pressure…

How to design EO/IR motion control that survives harsh environments: 5 conditions to plan for >

Electro-Optical/Infrared (EO/IR) Systems are used to provide long distance visual and thermal imaging for a variety of applications. Often used in satellites, planes, and military applications, there are two main components found in EO/IR systems:…
Overcoming the Limitations of Missile Design

Overcoming the Limitations of Missile Design >

Missiles operate in some of the most demanding conditions. They can experience massive heat flux when going through the layers of the earth’s atmosphere and because of the sheer speed that the missile is traveling at. With speeds in excess of 10,000…

Conventional slotted vs. slotless motors: which is better for low-speed, high-torque applications? >

What's the best way to achieve high torque and smooth operation at relatively low speeds, as required for EO/IR applications? Read our blog to find out.
Kollmorgen Motors for Defense: Proven Processes, Reliable Delivery

Kollmorgen Motors for Defense: Proven Processes, Reliable Delivery >

Few business challenges are as formidable and complex as winning a defense contract. Program specifications, contractual obligations and provisioning requirements are all far more demanding than practically anything encountered in the civilian…
Missiles and Guided Munitions Application Overview

Missiles and Guided Munitions Application Overview >

With industry-leading technology since the 1960’s, Kollmorgen has been helping innovate missile systems and smart munitions worldwide.