Skip to main content
Success Story | 2 minute read

Keiding Reinvents Custom Packaging

Kollmorgen Delivers Power and Precision

Keiding, Inc., leverages AKD® servo drives and AKM64L servo motors on a new molding machine to fuel state-of-the-art molded fiber packaging.

Fast Facts

Application:
Molded Fiber Packaging

Solutions Implemented:
AKD® drives with EtherNet/IP
AKM servo motors

Customer Since:
2017

Challenge and Results

Keiding pioneered the molded packaging industry in 1939, but in 2017 they were still operating machinery that had been built in the 1950s on a daily basis. As competitors entered the market using modern machinery, Mike Gehl, Keiding’s fourth-generation president, led the charge to build new machines by implementing industry expertise alongside new servo drive technologies. The result is a custom molding machine, which stands within the existing footprint of the original machinery, but also increases their customization capabilities. 

Dean Kindrai of Neff Engineering and the liaison between Keiding and Kollmorgen described the conditions and requirements, “The loads are relatively high, some of the required moves are quick, and where the motors are located, there is a relatively high ambient temperature and high humidity.” With a firm grasp on the unique challenge in front of them, the team decided to replace old pneumatic systems with four Kollmorgen AKD drives with Ethernet IP interface and AKM64L servo motors with integral shaft seals. 

Solutions

The partnership between Neff Engineering and Kollmorgen support engineers enabled the Keiding team to increase production efficiency, reduce maintenance and downtime, and attract new customers.

Advantages of Servo Motors over Pneumatic Systems

  • Operators can adjust the speed of moves easily based on the specific product being run via the PLC
  • Adjust the stroke lengths based on the product being run via the PLC
  • Change from box motion to arching motion to improve cycle time
  • Add a profile to the transfer that helps the product form better and dry faster
  • Eliminate binding common in machines with multiple air cylinders

Gehl states, “With the new machine, we’re able to make parts we were never able to make before.” In the past, Keiding’s production facility ran four 24-hour days each week, but with production at full capacity they are making the move to run 24 hours per day, 7 days per week. Faster machines, driven by precision motor control coupled with 3D printing tooling expertise, have put Keiding on a growth track that will keep them ahead of the game. They are using Kollmorgen technology to break the mold in the mold making business. 

ABOUT KOLLMORGEN

Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact [email protected] or call us at 540-633-3545.

Download as PDF
molded packaging prototype

Molded Packaging Prototype

Recycled Paper Gantry

Combined teams from Keiding and Neff built the gantry used to form recycled paper into the desired shape.

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production

Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production  >

One important stage in manufacturing lithium-ion batteries for electric vehicles is seal-welding the positive-terminal top cap to the battery shell. Laser welding is the ideal technology for this purpose, but it requires precise motion, speed and…
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…

Stop, hold and go safely: Motion tuning for vertical loads >

When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.

What are the Five Major Components of a Brushless Servo Motor >

Servo motors are used in numerous markets to power machines, instruments, robots, and other factory automation applications. This blog addresses five major elements of a conventional brushless DC servo motor: the rotor, stator, bearings, feedback and…