Skip to main content
press_release | Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products |
|
minute read

Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products

RADFORD, VA., 7/20/2023 — Kollmorgen, a global leader in motion control systems, today announced the launch of Kollmorgen Express Delivery. This new designation identifies highly popular motion products — including some of the most-requested configurations and options — that Kollmorgen is ready to deliver within an accelerated timeframe.

Machine builders have always benefited from Kollmorgen’s wide range of standard product configurations, features and options. This broad portfolio serves the unique needs of many diverse industries and applications but can create challenges for rapid delivery, especially when material supplies are constrained. However, with Kollmorgen Express Delivery, customers can now configure a servo system including specific configurations of AKM motors, AKD2G drives and matching cables, and take delivery of the system in as little as six weeks. For customers who only require an AKM motor, delivery times are as little as 4 weeks.

Over the past two years, Kollmorgen has invested significant resources to upgrade manufacturing plants and processes to meet urgent customer needs, and to assemble a team of the industry’s most accomplished operations and supply-chain talent. Manufacturing investments include enhanced production line automation, updated equipment and infrastructure, optimized plant workflows, advanced manufacturing analytics systems, and an ongoing commitment to rigorous lean production processes that drive quality and eliminate waste.

To create Kollmorgen Express Delivery, the company has optimized specific production lines for the purpose of manufacturing, modifying as necessary, and delivering in-demand products on an accelerated schedule. Kollmorgen will continue to monitor the success of the Express Delivery program and add additional product selections and variants to meet customer demand.

“Kollmorgen Express Delivery is just one example of how our recent investments in people, technology and processes are paying off ,” said James Woodall, Director of Operations. “We’ve always been committed to providing world-class motion quality and performance, and now our customers and distributors are gaining those benefits on a significantly faster delivery schedule.”

Kollmorgen Express Delivery is available to distributors and customers in North America. To learn more about the specific products available today, and to take advantage of Kollmorgen Express Delivery immediately, contact a Kollmorgen distributor or area sales manager, or visit www.kollmorgen.com/en-us/landing/kollmorgen-express-delivery.

About Kollmorgen

Kollmorgen, a Regal Rexnord brand, has more than 100 years of motion experience, proven in the industry’s highest-performing, most reliable motors, drives, linear actuators, AGV (Automated Guided Vehicle) control solutions, and automation control platforms. We deliver breakthrough solutions that combine exceptional performance, reliability and ease of use, giving machine builders an irrefutable marketplace advantage.

Functional Safety 101: The What, Why and How

Mandates and regulations aside, more customers are demanding functional safety. But no two applications are exactly the same, and there isn’t a one-size-fits-all solution. This whitepaper reveals how equipment manufacturers can stay up to speed.

Learn More

Monitoring and controlling brakes through on-drive functional safety technology

How can you ensure the safety of vertical loads while complying with ISO 13849-1? On-drive safety functions offer a no-compromise way to simplify brake testing.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Functional Safety 101 White Paper

Functional Safety 101: The What, Why and How >

Mandates and regulations aside, more customers are demanding functional safety. But no two applications are exactly the same, and there isn’t a one-size-fits-all solution. This whitepaper reveals how equipment manufacturers can stay up to speed.
Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging

Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging >

Kollmorgen's expertise in motion control components for packaging machinery helped Packsize tackle demanding challenges to create game-changing packaging automation solutions.

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Ground satellite 

AKD2G 24A Data Sheet >

Kollmorgen’s new AKD2G 24A servo drive delivers 3x the continuous current capacity and offers a rich feature set for simple integration in complex applications. 
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…
Kollmorgen White Paper, Monitoring and controlling brakes through on-drive functional safety technology

Monitoring and controlling brakes through on-drive functional safety technology >

How can you ensure the safety of vertical loads while complying with ISO 13849-1? On-drive safety functions offer a no-compromise way to simplify brake testing.

Stop, hold and go safely: Motion tuning for vertical loads >

When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.

5 Key Reasons to Consider an Upgrade to AKD2G Servo Drives >

Advances in processor technology for servo drives continue to expand the features and capabilities they offer. Choosing a new drive or control system over an existing system ultimately depends on the application requirements. The AKD2G servo drive…