Skip to main content
Success Story | 2 minute read

System Group

OPTIMIZED EFFICIENCY AND SAFETY IN LOGISTICS WITH KOLLMORGEN TECHNOLOGY

The collaboration between Kollmorgen and Gruppo System Spa resulted in the creation of an AGV vehicle which was 100% customized for a “big player” in the automotive sector: from now on their European sites will use bilateral AGV systems for warehouses and counterbalanced AGVs for the transportation of coils.

The system was built by Gruppo System Spa, an international leader in the manufacture of technological solutions for decoration, storage, packaging, palletising and transport goods throughout a plant or warehouse, using Kollmorgen technology. “Our client’s requirement,” comments Mauro Iacconi, Sales Manager for the AGV Dept. at System Spa, “was to have an automated and flexible warehousing system where an equally flexible conveyor-elevator would be deployed which would not be restricted to a specific warehouse and therefore, if necessary, could be moved elsewhere.” The proposed solution was tailored for a warehouse with a conventional shelving system where each side of the warehouse has double depth shelves with a free corridor in the middle where an AGV vehicle with bilateral forklifts has been installed; it is powered by two loading bays, manually handled by an operator (the presence of an operator was the client’s request). The circulation is managed by a supervisor with an NDC8 navigation system and assisted by WMS (Warehouse Management System) software: the result is improved handling times and thus enhanced productivity. The three vehicles manufactured for the European sites are already operative and thanks to their efficiency the customer was able to optimize the organization of the facility and to eliminate errors in the management of product storage and handling. The level of security was also improved, they can now move products in areas of the warehouse that are subject to potential safety risks without involving staff. “Following the European success story, we are confident that we will be able to repeat this type of system in other areas around the world and we are already working in this direction. We are extremely satisfied with Kollmorgen AGV systems: the flexible movement offered by the system-guided laser was a ‘must’ for our client. After all, pursuing deliverable flexible solutions reflects our corporate policy,” says Iacconi.

AGVs are completely self-driven: AGVs (Automatic Guided Vehicles) are automatic vehicles, ideal for moving goods and products within a plant, saving you time, energy and space in the logistics business. AGVs move independently, automatically and without the need of an operator or fixed structures on the floor, thanks to laser, magnetic and multi-navigation guidance systems that ensure the highest degree of flexibility for possible future developments of a facility. There are many industries in which AGVs can be used such as: ceramics, logistics, engineering, food & beverage, tissue, automotive, work stations, pharmaceuticals and warehouses with shelves.

Kollmorgen is a leading global provider of systems for AGV management: deep knowledge and skills together with a full range of hardware, software and navigation technologies are the winning combination that contribute to the repeated success of this company every day.

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.