Servo Controls Deliver Performance Benefits for Medical Imaging Systems

Medical imaging technology has rapidly advanced in recent years, increasing the speed and resolution of the images it produces. These advances have shifted the limiting factor on the time required to complete a scan and the quality of the resulting image from the imaging technology to the motion control system. As a result, medical imaging original equipment manufacturers (OEMs) have begun looking for alternatives to the AC induction motors traditionally used to position imaging gantries.