Skip to main content
Success Story | 2 minute read

MEDICAL: AKM, KBM, AKM & AKD-One Cable Package in the Medical Industry

HIGH IMPACT CUSTOMIZED SOLUTIONS

Interconnected engineering service increases productivity and creates tangible added value

Kollmorgen MEquadrat AKD-AKM One Cable Package

MEquadrat AG is a start-up that has been providing highly specialized solutions for four years as a mechatronics service provider, particularly in the laboratory and medical areas. Interdisciplinary thinking plays a fundamental role in this company’s product development activities. Original ideas related to implementation, efficient development and customized support also characterize the collaboration they had with drive specialist Kollmorgen on their new production module for the medical sector. Kollmorgens backlash-free direct drive solution allows exact synchronicity and concentricity with maximum precision up to 2 µm, and is more cost-effective.

One of the founding concepts of the service company MEquadrat AG, situated in the municipality of Root in Lucerne, is networked thinking and the creation of new machines and systems that meet its customers’ needs through consistency in the software used, the sophisticated mechanical and electronic components, and the associated increase in the degree of automation. One thing is clear for Stefan Nyffenegger, a member of the executive management team at MEquadrat AG: “The interlock between the mechanics, electronics, and soft-ware is the key to innovative products and higher productivity. We also break new ground with our unconven-tional approach, as can be seen with the current project for a machine module that is designed for processing thin-walled material in the medical sector”.

A difficult objective: Precise clamping despite high levels of rotation
Kollmorgen MEquadrat KMB Kit EN The two-sided and torsion-free clamping of highly sensitive glass and aluminum tubes is a particular challenge for the production module developed and constructed in Root. The product diameter ranges from between around one millimeter to 20 mm, with very thin wall thicknesses of around one-tenth of a millimeter. Cutting and joining processes are carried out on the sensitive hollow rod material. The high speed for the material clamped on both sides in the process requires absolute precision in terms of the synchronicity.

Developing the overall module in such a compact manner in accordance with the customer’s strict specifications required a highly meticulous and extremely precise drive system for the spindles in the workpiece feeder mechanism and for the relevant process steps with the clamped product. Stefan Nyffenegger highlights: “With the KBM kit motor solution from Kollmorgen we have found the perfect solution for our needs, as the product can be guided through the drive in a fluid process thanks to the large hollow shaft.”

 

Collaboration on an equal footing for unconventional solutions
The engineers at MEquadrat already had the idea of selecting a direct drive as they were designing the drive system. Their intention was to use an existing modular design in order to meet the precision requirements and to guarantee implementation on a time and cost-efficient basis.

But it became apparent that a rotor and a stator with the full functionality of a servo drive should be used as a result of the compact packing density and complexity of this assembly. In the end, the company decided the best solution was from Kollmorgen. The experts at the drive manufacturer were ready for any special requests. Decisions at the implementation stage for this project were made very quickly, as the experts from both com-panies collaborated with each other on an equal footing. The synchronicity however remained a problem. But a few ideas were developed for this and the product selection was narrowed down during some initial telephone discussions. The Key Account Manager at Kollmorgen, Martin Zimmermann, and his colleagues provided their full support: “When MEquadrat only requested the rotor and the stator for the feeder unit in this project, we knew that a mechatronics engineer would need to focus on the motor in greater detail. You have to have con-fidence when trying new things like in this project, which requires mutual and absolute trust”.

Kollmorgen MEquadrat SteffanNyffenegger MartinZimmermann EN

Aside from the time pressure and the extreme requirements related to precision in the functional specifications, there was another additional crucial challenge related to the medical technology: “The drive solution must be free from abrasion and lubricant, and we weren’t able to carry out any experiments at the implementation and commissioning stages for the mechanics and software”, says Nyffenegger. All of the components provided in this machine module therefore had to be tested and shown to be absolutely reliable.

The interaction of the direct drive with AKD Drives and the controllers from National Instruments (NI) enables extremely precise positioning. The cycle times in the current regulator are around 670 ns, and are just 62.5 µs in the speed regulator. Nyffenegger stresses: “This allows us to achieve optimum synchronicity in line with these high dynamic requirements. As such this drive combination represents the optimum price-performance ratio.”

Precise positioning with plug-and-play solutions
The crucial thing here that the two synchronized axes achieve extremely precise concentricity of 2 µm. Nyffenegger adds: “We’re talking about accuracy ranges that are otherwise only seen in spindle axes in large production plants.” The high speed was another of the major challenges in this project. There are systems on the market that “can indeed clamp sensitive products such as these at the required level of accuracy, but they often lose their clamping force from 500 rotations per minute. I haven’t seen any comparable product on the market that maintains its full clamping force at 3000 rpm!” highlights Nyffenegger.

The “AKM” drive with single-cable solution and SFD feedback were selected for the linear axis in the machine design. The components now just needed to be put together and everything fitted perfectly.

The resolver method as a single-cable solution is one of the drive expert’s specialties aimed at making opti-mum use of the robustness of the resolver. Nyffenegger stresses: “The wiring required in the AKM motor is also minimal here as a result. Highly compact cable carriers can also be used which really are sensational for tight spaces.”

Kollmorgen MEquadrat AKD-AKM One Cable Package Linear Axis Kollmorgen MEquadrat Direct Drive  

 

Summary: Achieving the objective using collaboration based on trust
The AKD one-cable package (controller & servo motor) is used for the components in the liner drive for the feeder mechanism. The major benefit with this is that the system comes from one source. Nyffenegger em-phasizes: “This way I don’t need to worry about any screw fittings or pins that do not fit. We just had to plug it in and get started, which also made the implementation time very short.” Integration of the precise drive tech-nology in the precise mechanics was therefore the central element in the very close and focused collaboration for this project. Keeping an eye on the costs – despite the required level of speed accuracy, the bearing and form tolerances for the mechanics and the fact that everything fits right from the word go, required a lot of mu-tual trust for both sides. Martin Zimmermann adds: “Our specific part in the project related in particular to our comprehensive recommendation as to how the customer can achieve its objective in an optimized and most cost-effective manner.”

One thing is clear for Stefan Nyffenegger: “We were also able to discuss ideas directly with the Kollmorgen product developers, and put forward our requests related to the shaft and hub connections. Sitting down at a table and discussing in order to find solutions, or discussing the design details on the phone, provided us with the assurance that everything would work correctly with the drive, and that we would be able to get things right the first time on this project.” The design phase alone for the machine took just three months, which is ex-tremely efficient. “The Kollmorgen part such as the installation of the axes and connection of the motor with full configuration and testing was completed within two days. This drive concept which was really customized to our needs worked out brilliantly for us. It fulfilled its objective, worked straight away, and met all of the requirements that we set ourselves for our customer.”

Kollmorgen MEquadrat AKD Servo Drive

Benefits of Use:  

  • High flexibility of the coordinated components
  • Integrated hollow shaft for special application predestines integration of a clamping system which maintains its clamping force even at 3000 rpm
  • Direct drive without any play or redundant mechanical parts allows exact synchronization and concentricity with the utmost precision up to 2 µm and is thereby hard-wearing
  • EtherCAT on board for simple implementation and integration (hardware and software) – also in LabVIEW
  • Excellent, comprehensive support from Kollmorgen from design through execution to commis-sioning
  • Easy conversion to different diameters
  • High process stability when increasing the degree of automation, achieving higher productivity

Products used: The following Kollmorgen motors (with a 1-cable system) and drives are used in the project:

AKM standard synchronous servo motors with permanent magnets. The powerful synchronous servo motors from the AKM series, which includes more than 500,000 standard models, are available in different fastening, connection, speed, and feedback versions and with lots of additional options.  

KBM frameless kit motors (modified by the customer in order to fit into the module). KBM frameless kit motors for rotary direct drive applications. The wide selection of frameless fit motors in the KBM series is the latest direct drive technology. They meet all of the requirements from machine constructors in terms of flexibility, power density, dynamics, lifespan, and simple installation.  

AKD & AKM one-cable package for easy integration. AKD servo controllers and AKM servo motors can be used in any application and are particularly cost-efficient one-cable solutions. The AKD servo amplifiers are fast, flexible, are suitable for a wide range of functions with Ethernet-based communication, and can therefore be integrated quickly and easily into any application. AKD enables plug-and-play commissioning and interfaces with all parts of the machine without barriers.  

Author/Pictures: Dipl.-Ing. Markus Frutig, TextConceptions.ch

About Kollmorgen
Kollmorgen is a leading supplier of integrated automation and driver systems, as well as related components, aimed at machine manufacturers all over the world. With over 70 years of experience in Motion Control Design and application, as well as its extensive knowledge in the areas of production standards and bespoke solutions, Kollmorgen provides prominent solutions in terms of performance, quality, reliability and ease of use. As a result, our clients gain indisputable leverage in the market. www.kollmorgen.com/uk - [email protected]

Download as PDF

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Scuba diver floating in deep ocean water, illustrating the extreme underwater conditions relevant to deep-sea motor technology

Reliable Motion at 4,000 Meters: IKM and Kollmorgen Advance Deep-Sea Motor Design >

Discover how IKM and Kollmorgen co-engineered a next-generation subsea system that reliably operates at depths of 4,000 meters under extreme conditions.
Signs You Should Consider a Frameless Motor in Your Machine

Signs You Should Consider a Frameless Motor in Your Machine >

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions?
English, IN
Redundant Servo Feedback: When Fail-Safe Positioning Is a Must

How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >

In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen Helps Salvagnini Build More Energy-Efficient Metal-Bending Machines >

Innovation, competency, service. Through 60 years in business, these three commitments have helped the Salvagnini Group achieve global leadership in the field of sheet-metal processing equipment. As the #1 worldwide supplier of panel benders, and one…

Compact, Efficient Motion Powers a Submersible Robot for In-Service Inspection of Fuel Storage Tanks >

Kollmorgen has helped many companies in a variety of industries increase performance, quality, throughput, and reduce costs. Read about our partners' successes here.

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Compliant Robotic Tooling Mitigates Risk and Delivers a Human Touch in Finishing Operations

How Compliant Robotic Tooling Delivers Safety and Precision in Finishing Operations  >

Force-controlled blending or finishing operations typically rely upon human operators who can provide subtle compliance in grinding, deburring or polishing. Unfortunately, these operations create inherent risks for these workers—from injuries to…