Skip to main content
Success Story | 2 minute read

Extending Design Life and Performance

Kollmorgen 2G Motion System Simplifies Set-Up in a 50+ Axis Meat Slicing Machine

Challenge

A major producer of food-slicing equipment needed a new servo system solution when the CAN fieldbus module used by its existing controller reached end of life and was no longer available. Exploring the latest fieldbus options, the engineering team chose an EtherCAT solution, which would require a new servo drive. The manufacturer engaged Kollmorgen to provide the technology and co-engineering expertise needed to deliver the required motion control.

The application is extremely complex, requiring the controller to communicate with the slicing machine’s 53 axes to control the feed rate, slicing operation, and positioning of the cut meat or cheese into a “shingle” arrangement ready for final packaging. To deliver the updated machine to market quickly and at the lowest possible cost, the customer wanted to minimize any design changes and to continue using Kollmorgen AKM family motors.

Solution

Already familiar with Kollmorgen’s motion-centric product and support capabilities, the customer opted to incorporate Kollmorgen’s next-generation 2G Motion System choosing the dual-axis AKD2G servo amplifier with EtherCAT connectivity from the many available fieldbus options.

As an early adopter of the AKD2G drive, the customer worked closely with a team of Kollmorgen application specialists to optimize the overall performance of the slicing machine. Given the large number of axes on this machine, the ability to set up each axis efficiently and to diagnose the system quickly was critical to success.

The customer found that the AKD2G’s integrated, front-mounted digital display, unique in the industry, made diagnosing fieldbus connections effortless. The AKD2G WorkBench user interface also significantly simplified setup and commissioning of the system compared to a competitor’s drive that the customer evaluated previously.

Results

The feature set of the Kollmorgen 2G Motion System provides several benefits in an upgraded food-slicing machine that will extend the performance and productivity of the original design over many years.

  • The single-cable design reduces labor and material costs for building the machine
  • The compact dual-axis AKD2G design reduces cabinet space requirements
  • The AKD2G integrated digital display reduces installation costs and simplifies setup and commissioning
  • Compatibility to operate the AKM family of servo motors at its full performance capacity eliminates the need for machine design revisions
  • Functional safety options are integrated in the drive, with no need to add additional components

“Our customer was thrilled with the innovative graphical display which simplified machine fieldbus commissioning.” - Arne Linder, Kollmorgen 2G Product Manager

Learn More

Ready to discover what the 2G Motion System can do for your machine?

Learn more

 

About Kollmorgen

Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, automated guided vehicle navigation software, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease of use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace of mind.

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.

Learn More

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever  >

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…
AKD2G Mentor Sessions: AKD2G Quick Setup Guide

AKD2G Mentor Sessions: AKD2G Quick Setup Guide & Advanced Configuration for AKD2G Dual Axis >

Need to get up and running with your new 2G system? It starts with the AKD2G Workbench software. This session will give you the fundamentals you need to create motion quickly, build confidence, and accelerate your productivity.
Functional Safety 101 White Paper

Functional Safety 101: The What, Why and How >

Mandates and regulations aside, more customers are demanding functional safety. But no two applications are exactly the same, and there isn’t a one-size-fits-all solution. This whitepaper reveals how equipment manufacturers can stay up to speed.
Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging

Kollmorgen helps packaging automation solutions provider meet the need for on-demand “right-sized” packaging >

Kollmorgen's expertise in motion control components for packaging machinery helped Packsize tackle demanding challenges to create game-changing packaging automation solutions.
Ground satellite 

AKD2G 24A Data Sheet >

Kollmorgen’s new AKD2G 24A servo drive delivers 3x the continuous current capacity and offers a rich feature set for simple integration in complex applications.