Skip to main content
Success Story | 2 minute read

Borealis uses AGVs to minimize operational cost and damage to goods.

By introducing automated guided vehicles (AGVs), Borealis in Stenungsund, Sweden, optimized both its product storage and dispatch efficiency with measurable results. Additionally, Borealis was able to increase its warehouse capacity by reducing the breadth of storage access lanes without increasing the risk of product damage.

Borealis provides polyethylene granules to a multitude of worldwide customers. These granules are the raw material used primarily by wire & cable and pipe manufacturers in large energy supply, oil and water pipeline projects. In 2001, Borealis improved its product handling by introducing automated guided vehicles (AGVs) provided by Rocla Oy, based on Kollmorgen technology. Thanks to laser guidance, AGVs operate with consistent accuracy and precise movements, greatly increasing safety and product integrity. At the same time, they have reduced labor and associated costs due to human error. To decrease the likelihood of accidents further, AGVs are restricted in areas where manual truck operations are underway. Borealis plans to use their AGV fleet for many years to come. “There are no competitive alternatives to AGVs,” says Peter Nyqvist of Borealis, “The warehouses will remain and the AGVs seem to be made like tanks, it is a pity that other electronic equipment cannot last as long.”

Kollmorgen, a leading manufacturer of driverless control technology, and Rocla Oy, a leading AGV system supplier, are strategic global partners in applications for automated transportation based on Kollmorgen’s AGV control technology. Kollmorgen control solutions are applied in more than 17,000 AGVs around the globe. Kollmorgen’s AGV control solution promises lower total costs for system integrators and end-users. It is applications independent, scalable and works with all AGVs, from the small and simple to the big and complex. It is also easy to integrate with host systems and material handling systems, and because the same platform is used everywhere, the same engineering skill set applies for all types of applications.

View the video:

Loading

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

NDC Flex

NDC Flex is a groundbreaking system that merges the efficiency of automated guided vehicles (AGVs) with the adaptability of autonomous mobile robots (AMRs). This hybrid approach ensures peak site productivity while mitigating risks related to potential disruptions.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.