Skip to main content
Success Story | 2 minute read

All-in-One: Servo drives in single-cable technology

All in one: One cable for all applications

Single-cable technology in servo drives: More than ten years of practical experience

The key theme of the discussions is essentially recognized; and the questions from neighboring disciplines, too. It goes something like: when does decentralized drive technology become worthwhile? When is it advisable to leave the frequency converters in the control cabinet? How high are the additional costs for shielded motor cables in centralized solutions when compared to higher device investment in robust "outdoor technology" with a high degree of protection? Machine and plant engineering now faces a similar question once again regarding the single-cable technology of servo motors. Kollmorgen brought this option onto the market ten years ago and now offers them as standard for synchronous servo motors of the AKM series.

At the time when Kollmorgen was developing the first AKM synchronous servo motor in single-cable technology, innovation was dominated by individual customer solutions. Today such close-knit partnerships in development are appropriately described using the term "co-engineering". The experience with single connection cables that has been amassed since then shows that the benefits of this trend in technology – which is currently being revived by other manufacturers – are only achieved in full if the conditions for application are appropriate.

Quick routing

Kollmorgen_onecable_AKM_Washdown_Food_ENThe benefits of connecting servo motors to their controllers with just one cable are enjoyed across the entire value-added chain in machine engineering. As encoder signals from the synchronous machine are physically transmitted via the motor cable, one interface is no longer necessary. The saving is realized through the omission of a cable and two plug connections. As a result, installation times are reduced, as is the space requirement for the cabling. The benefits have their price, of course, and this is in the cables themselves. Motor and encoder cables form part of the standard portfolio of recognized cable manufacturers. The same goes for connectors. The high production quantities combined with established technologies have a natural cost-reducing effect. However, if feedback and motor cables are inserted into a casing, then special attachments, impedances and particularly special shieldings are necessary. Solutions of this kind are thus no longer to be described as "market-standard" – with a corresponding impact on commissioning times and altogether more convenient and fault-free engineering, which is not ordinarily available with traditional resolvers. An additional benefit: The monitoring of the temperature sensor in the motor is integrated within the SFD via the digital position feedback, also without additional cabling work. 

If an application renders higher feedback system resolutions necessary, then a servo motor with Hiperface DSL interface simply comes into use – and without changing the cables. Kollmorgen has designed the single-cable servo solution so well that a universal cable-type can transmit the signals both from the digital resolver SFD and from the digital encoder. Kollmorgen_onecable_Smart Feedback Device_ENThe advantage of this multi-functionality: One cable for everything means fewer warehousing costs, reduced variance in material planning and documentation, and cheaper purchasing opportunities from higher volumes. In their basic versions, the AKM motors are equipped with a two-pole hollow-shaft resolver and, together with the AKD servo controller, with the digital SFD resolver interface that has already been mentioned. By way of options there are high-resolution Hiperface/DSL, BISS, or EnDat encoders and a Comcoder (incremental encoder with commutation). The variety of the price. Ignoring monetary aspects, cable lengths of over 50 meters are viewed critically, because with such systems they lead to faults. Additionally, continuously increasing integration as a whole is viewed sceptically by the cable manufacturers. For example, if one single wire breaks, then the whole cable has to be replaced, even though the rest is still functioning perfectly.

SFD: the digital resolver interface

As part of total costs of ownership and life-cycle costs, Kollmorgen has devised a solution for its own products that brings savings to the customer from the first meter onwards between motor and servo controller. Compared to other industry solutions distance is shorter, because Kollmorgen found a way to continue using resolvers, instead of more expensive feedback systems, from the very beginning. In this regard, using the Smart Feedback Device developed around ten years ago, the inexpensive yet robust technology becomes a digital feedback system with 24Bit resolution on the motor and regulator. The main task of the digital resolver (SFD interface) is to convert the analog encoder information internally into an interferenceresistant, purely digital RS-485 signal. With the conversion from analog to digital, Kollmorgen clears the way for being able to address the motors in the automation system, for example. The company's own SFD also boasts an EEPROM which has saved all relevant motor data as an electronic ID plate.Kollmorgen_onecable_AKDPDMM_EN This configuration allows automatic setup on the controller and ID plate recognition with all specific motor parameters in the controller. In practice, users benefit from shorter feedback systems ensures that drive solutions can be designed functionally and therefore also price-competitively, even in single-cable connection technology, scaled from a standard kit of motors and servo controllers and beyond. In machine and plant engineering, standardization brings you the advantage of a reduction in parts diversity, and thus also the related costs of stockpiling and keeping spares. With regard to performance, with 28 housing and length combinations the AKM series covers a wide range of applications with holding torques of 0.16 to 180 Nm. Speeds of up to 8,000 rpm also enable use in high-speed applications. Kollmorgen_onecable_singlecable_ENDue to the high power densities, the motors can be compared with small power packs.

The Bottom Line

The greatest benefit is derived from single-cable technology in machines that are spread out spatially with single axes that are also distributed and have long cable lengths. Long routes are also the key issue with decentralized drive technology, with the difference that the servo controller is placed right next to the motor or is integrated directly inside the motor. As feedback signals that are critical to functioning are to be transmitted with the new trend in single-cable connection technology, increasing importance is placed in the issue of shielding and compensation with this installation technology. Power cables that have been established to date are therefore not to be taken into consideration. Instead, specially shielded cables with modified impedances are used. 

 Kollmorgen_onecable_JörgPeters_EN

 

 

 

About Kollmorgen

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise. Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use, giving machine builders an irrefutable marketplace advantage.
Please contact us for more information.

 

Download article as PDF

Download as PDF

AKM Washdown and Food Grade

AKM Washdown and Washdown Food Series servomotors incorporate a protective 2-K coating, IP67-rated seals, stainless steel hardware, special greases and other materials designed for applications such as food, beverage and pharmaceutical processing where hygiene and frequent cleaning are critical requirements.

Learn More

The Difference Between Continuous Ratings and Holding Continuous Loads

When correctly sizing AC servo motors, it’s important to avoid miscommunication issues. Learn the critical terminology around sizing that leads to safe, reliable operation.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.

Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? >

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…
 The Difference Between Continuous Ratings and Holding Continuous Loads

The Difference Between Continuous Ratings and Holding Continuous Loads >

When correctly sizing AC servo motors, it’s important to avoid miscommunication issues. Learn the critical terminology around sizing that leads to safe, reliable operation.
Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…
Kollmorgen AKM Servomotor Catalog

Kollmorgen AKM Servomotor Catalog >

Kollmorgen AKM Series Catalog - The Most Versatile Synchronous Servo Motor in its Performance Class

AKM Washdown Datasheet EN revC >

AKM Washdown Datasheet Flawless Hygiene and a Compact Design – Powerful and Saves You Money

Alesa - Grinding Machine - Cutting edge: The shark’s teeth >

Saw blade manufacturer Alesa develops its own grinding machine with Washdown servo motors from KOLLMORGEN with single-cable connection technology.