Skip to main content

Kollmorgen AKM Series Selection Guide

The Most Versatile Synchronous Servo Motor in its Performance Class

Kollmorgen’s AKM family of servo motors gives you unprecedented choice and flexibility from a wide range of standard products so you can select the best servo motor for your application. Download the AKM Selection Guide to find out more.

Download as PDF

Fill out this short form

to view this Document

-OR-

Login / Register

to gain access to Kollmorgen content

Privacy Statement - By sending us your contact details you agree that your personal data/user behavior can be electronically stored and processed. If you no longer wish to receive the enewsletter, you can unsubscribe at any time.

AKM™ Series Servo Motor

Our best-in-class, high-performance servomotors offer a wide range of mounting, connectivity, feedback and other options. More than 500,000 standard models are available along with co-engineered modifications to suit almost any application requirement.

Learn More

AKM Washdown and Food Grade

AKM Washdown and Washdown Food Series servomotors incorporate a protective 2-K coating, IP67-rated seals, stainless steel hardware, special greases and other materials designed for applications such as food, beverage and pharmaceutical processing where hygiene and frequent cleaning are critical requirements.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…

Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? >

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…
Printing Machine

Direct Drive Motors Improve Flexographic Printing Performance >

Recent work done by Kollmorgen—a global leader in manufacturing motor and motion solutions—has shown that it is possible to synchronize components within the flexo printing process without mechanical transmission by using closed loop control…

How to Customize a Servo Motor - Standard vs Custom >

When and how to customize a standard servo motor depends on the predicted benefits derived from the customization that should include a solution tied to form, fit, and function. Learn more.
Kollmorgen webinar, What is a Servo Motor?

What is a Servo Motor? >

When researching motor options for an application, one type that often comes up is “servo” motor. Many manufacturers expand and add descriptions like AC and brushless. What do these terms mean and what exactly is a servo motor?

How to Select a Servo Motor >

There are several considerations when selecting a servo motor for a specific application, such as the required speed, torque or force, motion profile, available physical envelope, and environmental factors. This means that the chosen motor solution…

How Does a Servo Motor Work? >

A servo motor is an electromechanical device that produces torque and velocity based on the supplied current and voltage. A servo motor works as part of a closed loop system providing torque and velocity as commanded from a servo controller utilizing…
Kollmorgen Helps Rapidly Scale CT Scanner Production, Kollmorgen

Reliable and Consistent Supply of Motion Systems >

When the world became aware of the COVID-19 outbreak first identified in Wuhan, China, it quickly became clear that greatly increased diagnostic capacity would be needed. Early in the outbreak, one of the world’s largest producers of diagnostic…
Better Cut Quality Through Improved Connectivity, Kollmorgen

Better Cut Quality Through Improved Connectivity >

A Turkish-based company was looking to improve the cost, cut quality and machine serviceability of their flagship plasma cutting machine. Kollmorgen engineers implemented an AKM/AKD system solution to provide faster indexing and settle times. By…