Skip to main content

Kollmorgen Support Network

How to configure a KAS application to use Multiple EtherNet/IP assemblies | 01 Apr 2016 | |

How to configure a KAS application to use Multiple EtherNet/IP assemblies

The following steps describe how to configure multiple EtherNet/IP assemblies using two PDMMs.  For the purpose of this example, the adapter PDMM will perform a loop back to the scanner PDMM.

Create the PLCOpen Adapter Application.

  1. Open the FieldBus Editor and create the Ethernet/IP Adapter network
  2. Insert the Master Port
  3. Insert a Slave/Data block, selecting the proper IO Object type, Instance, and Size.  Repeat this step for each data block.image
    image
  4. Add a subprogram (EthernetIP) and variables to loop the received data back to the scanner
    image
  5. Compile, download and run the adapter application.

Create the PLCOpen Scanner Application.

  1. Open the FieldBus Editor and create the EtherNet/IP Scanner network.
  2. Insert the Master Port, setting the IP Address of the Server to the IP address of the Adapter Controller
    image
  3. For each assembly add the variables.  NOTE: For the Originator to Target (O -> T) verify that the 32 bit header is enabled.
    image
  4. Compile, download and run the scanner application.

About this Article

Carol Wesolowski