Skip to main content
press_release | Unlock fast-track AGV commissioning with Cirrus – the latest innovation from Kollmorgen -

Europe

|
|
minute read

Unlock fast-track AGV commissioning with Cirrus

Cirrus, the latest commissioning innovation from Kollmorgen, is a cloud-based solution that speeds up and streamlines AGV installations. With its smart features and easy-to-use interface, Cirrus can help accelerate your business by enabling efficient use of key resources in the commissioning process – both on-site and remote.

Streamline your commissioning

By simplifying the tuning and verification of layouts via an easy-to-use interface, Cirrus brings a step change to the commissioning process, providing two important workflow benefits. The flexibility of either remote or on-site operation, and the further advantage that only basic AGV and load handling knowledge is needed by the installation team. With the opportunity to deploy the commissioning team either remotely or on-site, and a wider pool of employees now empowered, the collaboration during tuning and verification becomes smoother, clearer and faster, resulting in commissioning time costs being slashed.

Easy onboarding and operation

Cirrus comprises two central strands: Cirrus Cloud and Cirrus Install.

Cirrus Cloud: Create and administrate projects at the office

  • Upload and download the current project layout.
  • Add users and assign them to projects.
  • Download updates made on-site, and import them to Layout Designer.

Cirrus Install: Easy and efficient commissioning on-site

  • Use the position of the vehicle to update points and stations in the layout.
  • Send local orders to test drive paths and stations.
  • Optimize drive paths.
  • Sync layout updates with Cirrus Cloud and colleagues at the office.
  • Enable both offline and online work.

Post-commissioning, Cirrus continues to import updates to the master layout and to confirm performance and capability KPIs.

Pioneers in AGV technology

The introduction of Cirrus adds another layer to the rich history of innovation in the AGV sector made by Sweden-based automation and motion specialist Kollmorgen. The company’s NDC Solutions automation kit is used across the globe by a growing number of vendors and providers.

“Our goal is to enable and optimize the automation journey for the AGV sector so that barriers to entry are reduced and opportunities are enhanced,” said Johanna Turesson, Director Product Management, Kollmorgen. We are therefore very proud of the possibilities that Cirrus brings to both the office and on-site environment to help speed up the commissioning process.”

She expanded on the benefits: “Firstly, it is so easy to use. Onboarding is fast, requiring no more than a couple of minutes, and while it requires some standard AGV knowledge and understanding, it enables various of on-site employees to participate in the commissioning process.”

“Second, the possibility to work both online and offline, either remotely or on-site, cuts lead times and travel costs, all supported by the ease of accessing layout information and updates anywhere, anytime.”

“Finally, as a cloud-based application, it creates a foundation of an online data-driven ecosystem that will benefit all stakeholders.”

Cirrus is available now. Interested parties should contact Kollmorgen

Automotive Manufacturing Logistics

Automotive manufacturing demands precision. AGVs ensure reliable material flow, reduce downtime, and improve efficiency—supporting just‑in‑time production while increasing accuracy and overall performance.
Learn More

NDC Layout Assistant

NDC Layout Assistant is a user-friendly application that lets you get instant feedback on your layout design even before running a simulation in the NDC8 system.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Illustration of automated warehouse environment

Textile Manufacturer Increases Efficiency by 45% with OKAGV & Kollmorgen >

See how a Southeast Asian textile manufacturer increased material handling efficiency by 45% and eliminated delivery errors with more than 100 AMRs and AGVs powered by OKAGV and Kollmorgen.

Interview with Kollmorgen AMS's Simon Bokesand on the Cyber Resilience Act >

The Cyber Resilience Act introduces several deadlines, including the September 11, 2026 start of mandatory vulnerability and incident reporting and December 11, 2027 full CRA compliance becomes mandatory for product with digital[BS1.1][MM1.2]…
NDC Layout Assistant

Kollmorgen Launches NDC Layout Assistant: Your Simple Solution for Smart Layout Analysis >

Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
NDC Layout Assistant Datasheet

NDC Layout Assistant Datasheet >

Maximize the layout performance with instant feedback on your layout design.
DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations

DB Schenker implements Jungheinrich AGVs with Kollmorgen technology for terminal operations >

DB Schenker in Borås has taken the next step in efficiently moving goods with tight timeframes by automating internal transports and increased productivity alongside improved safety and reduced production damages. The terminal has successfully…
Bring’s 3PL Flow Elevated: 173 Pallets/Hour with Kollmorgen & Rocla

Bring’s 3PL Flow Elevated: 200 Pallets/Hour with Kollmorgen & Rocla >

Bring Logistics, a leading third-party logistics provider in the Nordics, has automated its Skedsmo Logistics Centre in Bergen, near Oslo, with the help from Kollmorgen’s partner Rocla. The 32,000 m² facility now operates with nine Rocla very narrow…
Kollmorgen + ifm

Is This the End of Manual Pallet Adjustments in Logistics? >

In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
CVC700SW Datasheet

CVC700SW Datasheet >

The CVC700 software is the heart of the AGV. The software functions supervise everything from vehicle navigation to communication with the AGV system controller and the interfacing sensors and actuators.