Skip to main content

Teach your AGVs what to do >

Learn your AGVs the smartest driveway with teach functionality.

Finding the best AGV supplier on earth - or next door >

Local or specialized AGV supplier? How to find the right one.
Kollmorgen Blog

Collaborative Robots (cobots) - Who Benefits? >

Collaborative robots are designed to work safely with and next to their human counterparts.  A subset of collaborative robotics has innovative safety techniques that completely eliminate the need for a safety barrier between the human and the…

Checklist for meetings with AGV suppliers >

Buying AGVs? Read this checklist to avoid the pitfalls.
Kollmorgen Blog

Optimize your stepper motor solution with a new tool from Kollmorgen >

We are excited to introduce the launch of a brand new product selection tool – Kollmorgen Stepper Optimizer. Optimizer provides multiple ways for you to discover what Kollmorgen stepper motor works best in your application. Comprised in the tool are…

What is horsepower and how is it utilized with servo motors >

Horsepower (hp) is a measure of power, which can be further described as the rate at which work is performed.  There are slightly different definitions for its conversion to the unit watts depending on the mechanism being described: mechanical,…

Italian design brought to you by Kollmorgen >

For many, “Made in Italy” is synonymous with Italian ceramic tiles, but did you know most tiles have been handled by “someone” other than Italian workers?

Driverless vehicles—a reality at Volvo already in 1973 >

Read the exciting story on how Volvo introduced AGVs in their production. Even if 1973 seems 100 years ago, the technology is more relevant than ever.

Meeting the ‘got milk?’ challenge in Europe's dairies >

Europe's second largest dairy company, Arla Foods, has been using AGVs in their facilities since 2009. Read more to see how Arla Foods ensures everyone "gets milk."

AGVs in the new industrial landscape >

The next generation of industries is facing new challenges. What role can Automated Guided Vehicles play?

Tips on How to Confidently Set Up Your Linear Motor System >

Linear motors fill an important role in providing a robust and high precision direct drive solution in many high performance applications.  In order to achieve the highest level of performance, the linear motor system must be commissioned…

Issues to Consider when Operating a Motor in a Vacuum >

Question: I need to operate a servo motor in a vacuum, what are some considerations?  Answer: In a word?  Outgassing.  You might think that proper motor sizing is a big issue, it always is, however if you can't conform to the other…

Meet a real pioneer in laser-guided AGVs >

In the mid-1970s, Tetra Pak started to use AGVs (automated guided vehicles) in their manufacturing and warehouse facilities.

Key Tips on Dealing with 64-bit data on Modbus Communications Devices that only Support 32-bit data >

Most of the AKD drive’s parameters have a 32bit data size, but some parameters have a 64bit data size.  Modbus communication on the AKD drive uses registers of a 16bit data size.  So for a 64bit parameter, it takes four registers to send…

That's One Small Step... 0.9 vs 1.8 Degree Step Angle >

There is a lot of discussion about the 1.8 degree step angle versus 0.9 degree step angle of industrial hybrid stepper motors.  Most stepper motors today have the standard step angle of 1.8 degrees, resulting in a 200 step per…